imx tcm address

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx tcm address

697 Views
alkeke
Contributor I

Hi,

i try setup M4 core on IMX6SoloX

I read the AN5317 pdf

I would like to write a linux device driver which load m4 core 

For this i notice we shall fill the TCM U on CortxA9 with the M4 binary

But regarding provided example code , the TCM U seems located at 0x007F8000

On the other hand , while reading Linux Tcm code (tcm.c)  (kernel 4.1.21) and Arm cordtex A9 reference manual

(armv7-a-r-manual.pdf)

it seems that we could could access TCMU at 0xFFFFE000

and use macro  tcm_itcm_present() wich read CP15 c0 register to determine TCM presence

The second options dont 't seems to work

Is it relative to Cortex-A9 implementation in IMX6 or something else like a remapping TCM capability ?

Thanks in adv

Al

0 Kudos
Reply
0 Replies