Hi,
I am working on imx rt1050 evk.I tried flashing default camera example from the below path:
C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565 using IAR.
Only backlight for LCD comes up.nothing comes up on LCD.
Camera images are not displayed on LCD.
What will be the issue ?
How can we check LCD and camera are working fine?
Is there any LCD example to check if it is working fine for imx rt1050?
Thanks and Regards
Rizwan Syed
Hi,
When using the camera on Rev. A of i.MX RT EVK boards, it will be required to add 0-ohm resistors on R217, R218, R220, R221, R222, R223, R224, R225, R226, R227, R228 and R229, as mentioned on “MIMXRT1050 EVK Board Hardware User’s Guide” document.
Hope this will be useful for you.Best regards!
/Carlos