imx_kk4.4.2_1.0.0-ga Compilation error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx_kk4.4.2_1.0.0-ga Compilation error

Jump to solution
9,060 Views
embedded_ashu
Contributor II

Hi,

I wish to compile Android Kitkat source https://community.freescale.com/docs/DOC-101561/version/3

As per the document provided there i follow the steps, after the configuration when i make the sorce i am getting error.

source build/envsetup.sh

lunch sabresd_6dq-user

make 2>&1 | tee build_sabresd_6dq_android.log

...

out/target/common/obj/PACKAGING/public_api.txt:23522: error 12: Class android.telephony.gsm.SmsMessage changed static qualifier

out/target/common/obj/PACKAGING/public_api.txt:23523: error 4: Added public constructor SmsMessage()

out/target/common/obj/PACKAGING/public_api.txt:23524: error 4: Added public method android.telephony.gsm.SmsMessage.calculateLength

out/target/common/obj/PACKAGING/public_api.txt:23525: error 4: Added public method android.telephony.gsm.SmsMessage.calculateLength

out/target/common/obj/PACKAGING/public_api.txt:23526: error 4: Added public method android.telephony.gsm.SmsMessage.createFromPdu

out/target/common/obj/PACKAGING/public_api.txt:23527: error 4: Added public method android.telephony.gsm.SmsMessage.getDisplayMessageBody

out/target/common/obj/PACKAGING/public_api.txt:23528: error 4: Added public method android.telephony.gsm.SmsMessage.getDisplayOriginatingAddress

out/target/common/obj/PACKAGING/public_api.txt:23529: error 4: Added public method android.telephony.gsm.SmsMessage.getEmailBody

out/target/common/obj/PACKAGING/public_api.txt:23530: error 4: Added public method android.telephony.gsm.SmsMessage.getEmailFrom

out/target/common/obj/PACKAGING/public_api.txt:23531: error 4: Added public method android.telephony.gsm.SmsMessage.getIndexOnSim

out/target/common/obj/PACKAGING/public_api.txt:23532: error 4: Added public method android.telephony.gsm.SmsMessage.getMessageBody

out/target/common/obj/PACKAGING/public_api.txt:23533: error 4: Added public method android.telephony.gsm.SmsMessage.getMessageClass

out/target/common/obj/PACKAGING/public_api.txt:23534: error 4: Added public method android.telephony.gsm.SmsMessage.getOriginatingAddress

out/target/common/obj/PACKAGING/public_api.txt:23535: error 4: Added public method android.telephony.gsm.SmsMessage.getPdu

out/target/common/obj/PACKAGING/public_api.txt:23536: error 4: Added public method android.telephony.gsm.SmsMessage.getProtocolIdentifier

out/target/common/obj/PACKAGING/public_api.txt:23537: error 4: Added public method android.telephony.gsm.SmsMessage.getPseudoSubject

out/target/common/obj/PACKAGING/public_api.txt:23538: error 4: Added public method android.telephony.gsm.SmsMessage.getServiceCenterAddress

out/target/common/obj/PACKAGING/public_api.txt:23539: error 4: Added public method android.telephony.gsm.SmsMessage.getStatus

out/target/common/obj/PACKAGING/public_api.txt:23540: error 4: Added public method android.telephony.gsm.SmsMessage.getStatusOnSim

out/target/common/obj/PACKAGING/public_api.txt:23541: error 4: Added public method android.telephony.gsm.SmsMessage.getSubmitPdu

out/target/common/obj/PACKAGING/public_api.txt:23542: error 4: Added public method android.telephony.gsm.SmsMessage.getSubmitPdu

out/target/common/obj/PACKAGING/public_api.txt:23543: error 4: Added public method android.telephony.gsm.SmsMessage.getTPLayerLengthForPDU

out/target/common/obj/PACKAGING/public_api.txt:23544: error 4: Added public method android.telephony.gsm.SmsMessage.getTimestampMillis

out/target/common/obj/PACKAGING/public_api.txt:23545: error 4: Added public method android.telephony.gsm.SmsMessage.getUserData

out/target/common/obj/PACKAGING/public_api.txt:23546: error 4: Added public method android.telephony.gsm.SmsMessage.isCphsMwiMessage

out/target/common/obj/PACKAGING/public_api.txt:23547: error 4: Added public method android.telephony.gsm.SmsMessage.isEmail

out/target/common/obj/PACKAGING/public_api.txt:23548: error 4: Added public method android.telephony.gsm.SmsMessage.isMWIClearMessage

out/target/common/obj/PACKAGING/public_api.txt:23549: error 4: Added public method android.telephony.gsm.SmsMessage.isMWISetMessage

out/target/common/obj/PACKAGING/public_api.txt:23550: error 4: Added public method android.telephony.gsm.SmsMessage.isMwiDontStore

out/target/common/obj/PACKAGING/public_api.txt:23551: error 4: Added public method android.telephony.gsm.SmsMessage.isReplace

out/target/common/obj/PACKAGING/public_api.txt:23552: error 4: Added public method android.telephony.gsm.SmsMessage.isReplyPathPresent

out/target/common/obj/PACKAGING/public_api.txt:23553: error 4: Added public method android.telephony.gsm.SmsMessage.isStatusReportMessage

out/target/common/obj/PACKAGING/public_api.txt:23554: error 5: Added public field android.telephony.gsm.SmsMessage.ENCODING_16BIT

out/target/common/obj/PACKAGING/public_api.txt:23555: error 5: Added public field android.telephony.gsm.SmsMessage.ENCODING_7BIT

out/target/common/obj/PACKAGING/public_api.txt:23556: error 5: Added public field android.telephony.gsm.SmsMessage.ENCODING_8BIT

out/target/common/obj/PACKAGING/public_api.txt:23557: error 5: Added public field android.telephony.gsm.SmsMessage.ENCODING_UNKNOWN

out/target/common/obj/PACKAGING/public_api.txt:23558: error 5: Added public field android.telephony.gsm.SmsMessage.MAX_USER_DATA_BYTES

out/target/common/obj/PACKAGING/public_api.txt:23559: error 5: Added public field android.telephony.gsm.SmsMessage.MAX_USER_DATA_SEPTETS

out/target/common/obj/PACKAGING/public_api.txt:23560: error 5: Added public field android.telephony.gsm.SmsMessage.MAX_USER_DATA_SEPTETS_WITH_HEADER

******************************

You have tried to change the API from what has been previously approved.

To make these errors go away, you have two choices:

   1) You can add "@hide" javadoc comments to the methods, etc. listed in the

      errors above.

   2) You can update current.txt by executing the following command:

         make update-api

      To submit the revised current.txt to the main Android repository,

      you will need approval.

******************************

make: *** [out/target/common/obj/PACKAGING/checkapi-current-timestamp] Error 38

Then as per suggestion i use make update-api

again i am getting the below error.

out/target/common/obj/PACKAGING/public_api.txt:23516: error 12: Class android.telephony.gsm.SmsManager changed static qualifier

prebuilts/sdk/api/19.txt:23496: error 9: Removed public method android.telephony.gsm.SmsManager.divideMessage

prebuilts/sdk/api/19.txt:23497: error 9: Removed public method android.telephony.gsm.SmsManager.getDefault

prebuilts/sdk/api/19.txt:23498: error 9: Removed public method android.telephony.gsm.SmsManager.sendDataMessage

prebuilts/sdk/api/19.txt:23499: error 9: Removed public method android.telephony.gsm.SmsManager.sendMultipartTextMessage

prebuilts/sdk/api/19.txt:23500: error 9: Removed public method android.telephony.gsm.SmsManager.sendTextMessage

prebuilts/sdk/api/19.txt:23501: error 10: Removed field android.telephony.gsm.SmsManager.RESULT_ERROR_GENERIC_FAILURE

prebuilts/sdk/api/19.txt:23502: error 10: Removed field android.telephony.gsm.SmsManager.RESULT_ERROR_NO_SERVICE

prebuilts/sdk/api/19.txt:23503: error 10: Removed field android.telephony.gsm.SmsManager.RESULT_ERROR_NULL_PDU

prebuilts/sdk/api/19.txt:23504: error 10: Removed field android.telephony.gsm.SmsManager.RESULT_ERROR_RADIO_OFF

prebuilts/sdk/api/19.txt:23505: error 10: Removed field android.telephony.gsm.SmsManager.STATUS_ON_SIM_FREE

prebuilts/sdk/api/19.txt:23506: error 10: Removed field android.telephony.gsm.SmsManager.STATUS_ON_SIM_READ

prebuilts/sdk/api/19.txt:23507: error 10: Removed field android.telephony.gsm.SmsManager.STATUS_ON_SIM_SENT

prebuilts/sdk/api/19.txt:23508: error 10: Removed field android.telephony.gsm.SmsManager.STATUS_ON_SIM_UNREAD

prebuilts/sdk/api/19.txt:23509: error 10: Removed field android.telephony.gsm.SmsManager.STATUS_ON_SIM_UNSENT

******************************

You have tried to change the API from what has been previously released in

an SDK.  Please fix the errors listed above.

******************************

1 Solution
2,230 Views
freewaymad
Contributor IV

Hi Ashutosh,

First, you need to make sure you using the correct Java version; something like this:

java version "1.6.0_45"

Java(TM) SE Runtime Environment (build 1.6.0_45-b06)

Java HotSpot(TM) 64-Bit Server VM (build 20.45-b01, mixed mode)

If not, I have found this to be the easiest way to get the correct version installed:

Installing The JDK

Add PPA to system

$ sudo add-apt-repository ppa:webupd8team/java


Download & install java

$ sudo apt-get update && sudo apt-get install oracle-java6-installer


CHECK

$ java -version

You should see something like:

java version "1.6.0_45"

Java(TM) SE Runtime Environment (build 1.6.0_45-b06)

Java HotSpot(TM) 64-Bit Server VM (build 20.45-b01, mixed mode)

If not (I have had trouble with this i the past), go to:

http://www.oracle.com/technetwork/java/javasebusiness/downloads/java-archive-downloads-javase6-41940...

(in your browser and manually download)

You will have to login or setup an account with Oracle if you do not have one.

Put the "jdk-6u45-linux-x64.bin" in the home directory.

Then we need to run the binary and move it to a shared location by opening a terminal and typing:

$ chmod +x jdk-6u45-linux-x64.bin

$ sudo ./jdk-6u45-linux-x64.bin

$ sudo mv jdk1.6.0_45 /usr/lib/jvm/

Now you have to install all binaries and give them highest priority, This will also overwrite the previous version of Java Binaries in your computer:

$ sudo update-alternatives --install /usr/bin/java java /usr/lib/jvm/jdk1.6.0_45/bin/java 1

$ sudo update-alternatives --install /usr/bin/javac javac /usr/lib/jvm/jdk1.6.0_45/bin/javac 1

$ sudo update-alternatives --install /usr/bin/javaws javaws /usr/lib/jvm/jdk1.6.0_45/bin/javaws 1

$ sudo update-alternatives --install /usr/bin/jar jar /usr/lib/jvm/jdk1.6.0_45/bin/jar 1

$ sudo update-alternatives --install /usr/bin/javadoc javadoc /usr/lib/jvm/jdk1.6.0_45/bin/javadoc 1

$ sudo update-alternatives --install /usr/bin/javap javap /usr/lib/jvm/jdk1.6.0_45/bin/javap 1  (EDIT - This is needed to compile Kit Kat 4.4)

Most of the time I get after these commands, basically the jdk is not there. Just run the binary and move it to a shared location using three commands above again and install and give them the highest priority again...its a pain, I know)

Now check if JDK 1.6 is selected on this:

$ sudo update-alternatives --config java

$ sudo update-alternatives --config javac

$ sudo update-alternatives --config javaws

$ sudo update-alternatives --config jar

$ sudo update-alternatives --config javadoc

$ sudo update-alternatives --config javap  (EDIT - This is needed to compile Kit Kat 4.4)

These six should all be selected.

Now JDK is configured! To check if it is done

Execute this is Terminal:

$ java -version

Output will be similar to this:

java version "1.6.0_45"

Java(TM) SE Runtime Environment (build 1.6.0_45-b06)

Java HotSpot(TM) 64-Bit Server VM (build 20.45-b01, mixed mode)

IF NOT, YOU MAY NEED TO RUN AGAIN

JDK is now configured. You can now delete or save somewhere else "jdk-6u45-linux-x64.bin"  that is in the home directory

(Full android setup here: https://community.freescale.com/message/421522#421522 ) This is for Ubuntu 14.04, but the JDK setup is the same.

NOTICE that you will need javap installed and given the highest priority to compile Kit Kat.

I hope this helps,


Dave


View solution in original post

0 Kudos
Reply
3 Replies
2,231 Views
freewaymad
Contributor IV

Hi Ashutosh,

First, you need to make sure you using the correct Java version; something like this:

java version "1.6.0_45"

Java(TM) SE Runtime Environment (build 1.6.0_45-b06)

Java HotSpot(TM) 64-Bit Server VM (build 20.45-b01, mixed mode)

If not, I have found this to be the easiest way to get the correct version installed:

Installing The JDK

Add PPA to system

$ sudo add-apt-repository ppa:webupd8team/java


Download & install java

$ sudo apt-get update && sudo apt-get install oracle-java6-installer


CHECK

$ java -version

You should see something like:

java version "1.6.0_45"

Java(TM) SE Runtime Environment (build 1.6.0_45-b06)

Java HotSpot(TM) 64-Bit Server VM (build 20.45-b01, mixed mode)

If not (I have had trouble with this i the past), go to:

http://www.oracle.com/technetwork/java/javasebusiness/downloads/java-archive-downloads-javase6-41940...

(in your browser and manually download)

You will have to login or setup an account with Oracle if you do not have one.

Put the "jdk-6u45-linux-x64.bin" in the home directory.

Then we need to run the binary and move it to a shared location by opening a terminal and typing:

$ chmod +x jdk-6u45-linux-x64.bin

$ sudo ./jdk-6u45-linux-x64.bin

$ sudo mv jdk1.6.0_45 /usr/lib/jvm/

Now you have to install all binaries and give them highest priority, This will also overwrite the previous version of Java Binaries in your computer:

$ sudo update-alternatives --install /usr/bin/java java /usr/lib/jvm/jdk1.6.0_45/bin/java 1

$ sudo update-alternatives --install /usr/bin/javac javac /usr/lib/jvm/jdk1.6.0_45/bin/javac 1

$ sudo update-alternatives --install /usr/bin/javaws javaws /usr/lib/jvm/jdk1.6.0_45/bin/javaws 1

$ sudo update-alternatives --install /usr/bin/jar jar /usr/lib/jvm/jdk1.6.0_45/bin/jar 1

$ sudo update-alternatives --install /usr/bin/javadoc javadoc /usr/lib/jvm/jdk1.6.0_45/bin/javadoc 1

$ sudo update-alternatives --install /usr/bin/javap javap /usr/lib/jvm/jdk1.6.0_45/bin/javap 1  (EDIT - This is needed to compile Kit Kat 4.4)

Most of the time I get after these commands, basically the jdk is not there. Just run the binary and move it to a shared location using three commands above again and install and give them the highest priority again...its a pain, I know)

Now check if JDK 1.6 is selected on this:

$ sudo update-alternatives --config java

$ sudo update-alternatives --config javac

$ sudo update-alternatives --config javaws

$ sudo update-alternatives --config jar

$ sudo update-alternatives --config javadoc

$ sudo update-alternatives --config javap  (EDIT - This is needed to compile Kit Kat 4.4)

These six should all be selected.

Now JDK is configured! To check if it is done

Execute this is Terminal:

$ java -version

Output will be similar to this:

java version "1.6.0_45"

Java(TM) SE Runtime Environment (build 1.6.0_45-b06)

Java HotSpot(TM) 64-Bit Server VM (build 20.45-b01, mixed mode)

IF NOT, YOU MAY NEED TO RUN AGAIN

JDK is now configured. You can now delete or save somewhere else "jdk-6u45-linux-x64.bin"  that is in the home directory

(Full android setup here: https://community.freescale.com/message/421522#421522 ) This is for Ubuntu 14.04, but the JDK setup is the same.

NOTICE that you will need javap installed and given the highest priority to compile Kit Kat.

I hope this helps,


Dave


0 Kudos
Reply
2,229 Views
embedded_ashu
Contributor II

Thanks Dave,

Its very helpful information.

Finally i am able to build it.

0 Kudos
Reply
2,229 Views
LuisCasado
NXP Employee
NXP Employee

Hello,

I got exactly the same issue in a clean Ubuntu installation. The problem was the version of Java in the Host. I corrected it following the User Guide link to community doc.

community.freescale.com/docs/DOC-98441

I did first "make clean” after correcting the Java to the right one. Then:

lunch sabresd_6dq-user

make 2>&1 | tee build_sabresd_6dq_android.log

I hope this helps.

Luis