imx-keypad wakeup from suspend on 6sl using linux 3.0.35

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx-keypad wakeup from suspend on 6sl using linux 3.0.35

2,032 Views
jayakumar2
Contributor V


Hi imx friends,

I'm using a 6sololite board with linux 3.0.35. I have been using the matrix keypad support and it is working fine. I am able to read the key input events in software with no problem. Thanks to everyone who helped make that work.

So now I'm trying to test suspend/resume. I have tested console based suspend/resume and this also works fine. The way I test that is:

# echo enabled > /sys/devices/platform/imx-uart.1/tty/ttymxc1/power/wakeup

# echo mem > /sys/power/state

PM: Syncing filesystems ... done.

PM: Preparing system for mem sleep

Freezing user space processes ... (elapsed 0.01 seconds) done.

Freezing remaining freezable tasks ... (elapsed 0.01 seconds) done.

PM: Entering mem sleep

Suspending console(s) (use no_console_suspend to debug)

Then I hit any key on serial console and it resumes.

udc suspend begins

USB Gadget suspend ends

add wake up source irq 59

add wake up source irq 58

add wake up source irq 51

PM: suspend of devices complete after 2.264 msecs

PM: late suspend of devices complete after 0.490 msecs

PM: early resume of devices complete after 0.341 msecs

remove wake up source irq 51

remove wake up source irq 58

remove wake up source irq 59

USB Gadget resume begins

fsl_udc_resume, Wait for wakeup thread finishes

dr_controller_run: udc enter low power mode

USB Gadget resume ends

PM: resume of devices complete after 123.276 msecs

PM: Finishing wakeup.

Restarting tasks ... done.

Okay, so all of that looks good. Now what I would like to do is to do the same thing from the keypad button. On non-imx boards, I'm used to using the wakeup flag with matrix-keypad driver to make this work. But on mx6, there is no matrix-keypad support, only imx-keypad support. In my code, I tried:

static int mx6sl_evk_keymap[] = {

        KEY(0, 0, KEY_POWER),

        KEY(1, 0, KEY_BACK),

        KEY(2, 0, KEY_F1),

        KEY(3, 0, KEY_F2),

...

static const struct matrix_keymap_data mx6sl_evk_map_data __initconst = {

        .keymap         = mx6sl_evk_keymap,

        .keymap_size    = ARRAY_SIZE(mx6sl_evk_keymap),

};

        imx6sl_add_imx_keypad(&mx6sl_evk_map_data);

Above ends up in:

drivers/input/keyboard/imx_keypad.c

which does:

        device_init_wakeup(&pdev->dev, 1);

So we know that the imx_keypad driver is enabling wakeup. But this doesn't seem to work for me. I can see that interrupts from the buttons are working fine during normal activity. Eg:

cat /proc/interrupts

114:          4       GIC  imx-keypad

121:          0       GIC  dvfs

130:          0       GIC  pxp-irq

Err:          0

root@imx6qsabresd:~# echo mem > /sys/power/state

PM: Syncing filesystems ... done.

PM: Preparing system for mem sleep

Freezing user space processes ... (elapsed 0.01 seconds) done.

Freezing remaining freezable tasks ... (elapsed 0.01 seconds) done.

PM: Entering mem sleep

Suspending console(s) (use no_console_suspend to debug)

<-- Here, I press all the buttons many times and no wakeup is activated.

Is there some iomux or pad setting that I need to do to make the keypad support wakeup from suspend? I would appreciate any advice/suggestions.

Thanks!

Labels (2)
Tags (1)
0 Kudos
Reply
2 Replies

1,367 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jaya

please try patch provided on

How to use the kpp for imx6q+android4.3?

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,367 Views
jayakumar2
Contributor V

Hi Igor,

Thanks for your reply. I was able to modify the patch to be suitable for my setup. In my case, I'm using the following pins for the buttons:

        MX6SL_PAD_SD1_CLK__KPP_COL_0,        

        MX6SL_PAD_SD1_CMD__KPP_ROW_0,       

        MX6SL_PAD_SD1_DAT1__KPP_ROW_1,

        MX6SL_PAD_SD1_DAT3__KPP_ROW_2,      

        MX6SL_PAD_SD1_DAT5__KPP_ROW_3, 

I modified my common to match the patch you linked to. My patch is therefore:

--- a/arch/arm/mach-mx6/board-mx6sl_common.h

+++ b/arch/arm/mach-mx6/board-mx6sl_common.h

@@ -484,14 +484,14 @@ static iomux_v3_cfg_t suspend_enter_pads[] = {

        /* PWM pads */

        MX6SL_PAD_PWM1__GPIO_3_23,

        /* SD pads. */

-       MX6SL_PAD_SD1_CLK__GPIO_5_15,

-       MX6SL_PAD_SD1_CMD__GPIO_5_14,

+//     MX6SL_PAD_SD1_CLK__GPIO_5_15, XXXjaya disable to allow resume

+//     MX6SL_PAD_SD1_CMD__GPIO_5_14, XXXjaya disable to allow resume

        MX6SL_PAD_SD1_DAT0__GPIO_5_11,

-       MX6SL_PAD_SD1_DAT1__GPIO_5_8,

+//     MX6SL_PAD_SD1_DAT1__GPIO_5_8, XXXjaya disable to allow resume

        MX6SL_PAD_SD1_DAT2__GPIO_5_13,

-       MX6SL_PAD_SD1_DAT3__GPIO_5_6,

+//     MX6SL_PAD_SD1_DAT3__GPIO_5_6, XXXjaya disable to allow resume

        MX6SL_PAD_SD1_DAT4__GPIO_5_12,

-       MX6SL_PAD_SD1_DAT5__GPIO_5_9,

+//     MX6SL_PAD_SD1_DAT5__GPIO_5_9, XXXjaya disable to allow resume

        MX6SL_PAD_SD1_DAT6__GPIO_5_7,

        MX6SL_PAD_SD1_DAT7__GPIO_5_10,

Unfortunately, with this change I still can't get resume from buttons to work. However, there is a change because now after the button press, and then resuming using console, I see the interrupt count for imx-keypad has increased.

# cat /sys/devices/platform/imx-keypad/input/input0/uevent

PRODUCT=19/0/0/0

NAME="imx-keypad"

PROP=0

EV=100013

KEY=2 0 0 0 0 0 0 40000000 0 0 18000000 0

MSC=10

MODALIAS=input:b0019v0000p0000e0000-e0,1,4,14,k9E,161,ram4,lsfw

# echo mem > /sys/power/state

PM: Syncing filesystems ... done.

PM: Preparing system for mem sleep

Freezing user space processes ... (elapsed 0.01 seconds) done.

Freezing remaining freezable tasks ... (elapsed 0.01 seconds) done.

PM: Entering mem sleep

Suspending console(s) (use no_console_suspend to debug)

so now I press button and it doesn't wakeup. But I use serial console resume and then check interrupt count.

wl1271: down

udc suspend begins

USB Gadget suspend ends

add wake up source irq 58

add wake up source irq 51

PM: suspend of devices complete after 9.865 msecs

PM: late suspend of devices complete after 0.500 msecs

PM: early resume of devices complete after 0.343 msecs

remove wake up source irq 51

remove wake up source irq 58

ddrMode=0, lvdsModeCe=0, lvdsMode=0, prev EPDC_TCE_CTRL 0x10, new val 0x40002

after write EPDC_TCE_CTRL 0x40002

USB Gadget resume begins

fsl_udc_resume, Wait for wakeup thread finishes

dr_controller_run: udc enter low power mode

USB Gadget resume ends

wl1271: firmware booted (Rev 6.1.5.50.69)

PM: resume of devices complete after 590.333 msecs

PM: Finishing wakeup.

Restarting tasks ... done.

# cat /proc/interrupts

           CPU0     

34:          0       GIC  sdma

51:          0       GIC  snvs_rtc

55:      22881       GIC  mmc0

56:      15351       GIC  mmc1

58:       1027       GIC  IMX-uart

63:          0       GIC  spi_imx

68:        274       GIC  imx-i2c

69:          0       GIC  imx-i2c

75:          0       GIC  usb_wakeup, fsl-usb2-udc

87:       1533       GIC  i.MX Timer Tick

112:          0       GIC  imx2-wdt

114:          2       GIC  imx-keypad

121:          0       GIC  dvfs

129:          4       GIC  fb_dma

130:          1       GIC  pxp-irq

391:        192      GPIO  wl1271

Err:          0

It looks like the problem is that there is still some configuration step that's missing. I noticed once the resume occurs, it says:

USB Gadget suspend ends

add wake up source irq 58

add wake up source irq 51

So it looks like the imx-uart is registered as a wake up source (irq 58) and that's why it works. But I can't see irq 141 registered as a wakeup source. So what's missing is registering a wakeup source. I'm now looking for where that needs to be done.

I checked that wakeup is enabled for keypad in sysfs:

# echo enabled > /sys/devices/platform/imx-keypad/power/wakeup

# cat /sys/devices/platform/imx-keypad/power/wakeup

enabled

Still looking for where wakeup source is configured.

Thanks!

0 Kudos
Reply