hi,
I not able to detect my monitor with HDMI cable.
when i am plugging HDMI cable to HDMI port in my i.mx6 board i am getting this warning :
imx-ipuv3 imx-ipuv3.0: WARNING: adapt panel end blank lines
please help
Thanks in advance.
regards
ikshwaku
Hi,
I have the same problem on my Linux 3.0.35 iMX6q. I use Buildroot 2014.02. In older buildroots I haven't got this warning. Until I merged to a newer version.
Is there now a solution for this??
Thanks
Andi
I'm having similar issue with my Sabre board from Boundary Devices. I'm using the Linaro Ubuntu Desktop version 12.05
I flash my board according to :
http://boundarydevices.com/running-linaro-ubuntu-on-i-mx6-sabre-lite-and-nitrogen6x/
how ever when I start it up then my display(HP ZR22w) is not being detected. I have tracked this down to something to do with the boot.scr in the boot partition. Basically if I change then line:
setenv bootargs "console=tty0 console=ttymxc1,115200n8 video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24 root=UUID=93047a55-33e3-4455-97fb-d7c399261e6c rootwait ro"
to
setenv bootargs "console=ttymxc1,115200n8 video=mxcfb0:dev=hdmi,1280x720M@60,if=RGB24 vmalloc=400M fbmem=28M no_console_suspend root=UUID=93047a55-33e3-4455-97fb-d7c399261e6c rootwait ro"
then recreate the bootscripts with the online tool :
http://git.boundarydevices.com/bootscript.php
and replace the boot.ini boot.scr and boot.txt
Then my display detects and can show the Ubuntu loggin, how ever it goes to sleep after ~20 sec flashing:
"Input Signal Out of Range Change Settings to 1920 x 1080 - 60Hz"
I can see the line:
[ 15.150540] imx-ipuv3 imx-ipuv3.0: WARNING: adapt panel end blank lines
being printed out in the serial console....
Can anyone see what I'm doing wrong?
Hi
Can you please indicate us the bsp release and the reference design board that your are using?
thanks.
-ni.
Hi,
Thanks for your reply..now i am able to resolve this issue... :smileyhappy:
regards
iksh
we just change the display settings for HDMI.