imx-ipuv3 imx-ipuv3.0: WARNING: adapt panel end blank lines

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx-ipuv3 imx-ipuv3.0: WARNING: adapt panel end blank lines

5,070 Views
Ikshwakuchauhan
Contributor II

hi,

I not able to detect my monitor with HDMI cable.

when i am plugging HDMI cable to HDMI port in my i.mx6 board i am getting this warning :

imx-ipuv3 imx-ipuv3.0: WARNING: adapt panel end blank lines

please help

Thanks in advance.

regards

ikshwaku

Labels (4)
0 Kudos
Reply
6 Replies

2,495 Views
andreaszeiler
Contributor III

Hi,

I have the same problem on my Linux 3.0.35 iMX6q. I use Buildroot 2014.02. In older buildroots I haven't got this warning. Until I merged to a newer version.

Is there now a solution for this??

Thanks

Andi

0 Kudos
Reply

2,495 Views
stefanpalsson
Contributor I

I'm having similar issue with my Sabre board from Boundary Devices.  I'm using the Linaro Ubuntu Desktop version 12.05

I flash my board according to :

http://boundarydevices.com/running-linaro-ubuntu-on-i-mx6-sabre-lite-and-nitrogen6x/

how ever when I start it up then my display(HP ZR22w) is not being detected.  I have tracked this down to something to do with the boot.scr in the boot partition.  Basically if I change then line:

setenv bootargs "console=tty0 console=ttymxc1,115200n8 video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24 root=UUID=93047a55-33e3-4455-97fb-d7c399261e6c rootwait ro"

to

setenv bootargs "console=ttymxc1,115200n8 video=mxcfb0:dev=hdmi,1280x720M@60,if=RGB24 vmalloc=400M fbmem=28M no_console_suspend root=UUID=93047a55-33e3-4455-97fb-d7c399261e6c rootwait ro"

then recreate the bootscripts with the online tool :

http://git.boundarydevices.com/bootscript.php

and replace the boot.ini boot.scr and boot.txt

Then my display detects and can show the Ubuntu loggin, how ever it goes to sleep after ~20 sec flashing:

"Input Signal Out of Range Change Settings to 1920 x 1080 - 60Hz"

I can see the line:

[   15.150540] imx-ipuv3 imx-ipuv3.0: WARNING: adapt panel end blank lines

being printed out in the serial console....


Can anyone see what I'm doing wrong?


0 Kudos
Reply

2,495 Views
NicolasIzquierd
Contributor III

Hi

Can you please indicate us the bsp release and the reference design board that your are using?

thanks.

-ni.

0 Kudos
Reply

2,495 Views
Ikshwakuchauhan
Contributor II

Hi,

Thanks for your reply..now i am able to resolve this issue... :smileyhappy:

regards

iksh

0 Kudos
Reply

2,495 Views
Trilokesh
Contributor I

can please let me know how you solved this issue

0 Kudos
Reply

2,495 Views
Ikshwakuchauhan
Contributor II

we just change the display settings for HDMI.

0 Kudos
Reply