Hi,
I'm using gstreamer to play RTSP stream and I seem to be getting this warning message on every frame.
I've had a look on "iMX6Q Reference Manual" and it says "SMFC0_FRM_LOST". What does this exactly mean and how do I fix this?
Thanks in advance.
It looks like FRaMe LOST situation occurs (I expect because IPU is overloaded).
Some information about it may be found in i.MX6 (Q) RM just before Table 37-36 (Error
Interrupts Summary) :
"The table below describes the error interrupts. The panic column indicates if this signal is
part of the logic generating the ipu_panic signal. The ipu_panic signal can be used for
indicating about errors that are result of data rate problems. Such problems may be a
result of the IPU running in slower clock then required by the use case. This signal can be
used in order to indicate the system that the IPU can't handle the desired data rate. In that
case the system may need to increase the clock to the IPU or simplify the use case."
Thanks for the reply. It's weird because I'm only receiving 1 stream of VGA @ 15FPS and I seem to be getting the error message on every frame but the video is showing up fine on the display.
I've had a look at the clock, it seems like IPU default clocks are set to 264MHz from the maximum of 266MHz? I'm not changing the clock at all so is it safe to assume it's set to near max speed?
You may refer to the next thread :