imx-image-full-imx8mpevk.wic.zst is not created

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx-image-full-imx8mpevk.wic.zst is not created

526 次查看
srinivas_123
Contributor II

I am using imx 8mplus lpddr4 evk. I build the yocto image for the latest BSP of  IMXLXYOCTOUG v.LF6.6.3_1.0.0. I successfully build the image but  imx-image-full-imx8mpevk.wic.zst file is not created. 

I know only wic.zst file is directly flashed into the sd card. without wic.zst file how to boot up the target.is it required to do any configurations in the new BSP MXLXYOCTOUG v.LF6.6.3_1.0.0 to create wic.zst file?

if anyone knows how to flash uboot, kernel,rootfs into sd card . please let me know.

Thanks&Regards

srinivas

 

0 项奖励
回复
4 回复数

516 次查看
Alejandro_Salas
NXP TechSupport
NXP TechSupport

Hello @srinivas_123 

Could you please share your steps to replicate by mi side?

 

Also, if possible the list of the files generated by Yocto.

 

Best regards.

Salas.

0 项奖励
回复

492 次查看
srinivas_123
Contributor II

Hello @Alejandro_Salas Screenshot from 2024-05-18 10-46-14.pngScreenshot from 2024-05-18 10-46-30.pngScreenshot from 2024-05-18 10-46-24.pngScreenshot from 2024-05-18 10-45-43.pngScreenshot from 2024-05-18 10-44-03.pngScreenshot from 2024-05-18 10-46-00.pngScreenshot from 2024-05-18 10-45-53.pngScreenshot from 2024-05-18 10-45-34.png

0 项奖励
回复

448 次查看
Alejandro_Salas
NXP TechSupport
NXP TechSupport

Hello @srinivas_123 

 

The image was generated successfully, you can see the file with extension .wic.zst.

 

You can decompress that file with zstd -d your_file.wic.zst command and you will have your pure wic file.

 

Best regards.

Salas.

0 项奖励
回复

494 次查看
srinivas_123
Contributor II

Screenshot from 2024-05-18 10-46-14.pngScreenshot from 2024-05-18 10-46-30.pngScreenshot from 2024-05-18 10-46-24.pngScreenshot from 2024-05-18 10-45-43.pngScreenshot from 2024-05-18 10-44-03.pngScreenshot from 2024-05-18 10-46-00.pngScreenshot from 2024-05-18 10-45-53.pngScreenshot from 2024-05-18 10-45-34.png

0 项奖励
回复