imx-image-full-imx8mpevk.wic.zst is not created

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx-image-full-imx8mpevk.wic.zst is not created

1,187 Views
srinivas_123
Contributor III

I am using imx 8mplus lpddr4 evk. I build the yocto image for the latest BSP of  IMXLXYOCTOUG v.LF6.6.3_1.0.0. I successfully build the image but  imx-image-full-imx8mpevk.wic.zst file is not created. 

I know only wic.zst file is directly flashed into the sd card. without wic.zst file how to boot up the target.is it required to do any configurations in the new BSP MXLXYOCTOUG v.LF6.6.3_1.0.0 to create wic.zst file?

if anyone knows how to flash uboot, kernel,rootfs into sd card . please let me know.

Thanks&Regards

srinivas

 

0 Kudos
Reply
4 Replies

1,177 Views
Alejandro_Salas
NXP TechSupport
NXP TechSupport

Hello @srinivas_123 

Could you please share your steps to replicate by mi side?

 

Also, if possible the list of the files generated by Yocto.

 

Best regards.

Salas.

0 Kudos
Reply

1,153 Views
srinivas_123
Contributor III

Hello @Alejandro_Salas Screenshot from 2024-05-18 10-46-14.pngScreenshot from 2024-05-18 10-46-30.pngScreenshot from 2024-05-18 10-46-24.pngScreenshot from 2024-05-18 10-45-43.pngScreenshot from 2024-05-18 10-44-03.pngScreenshot from 2024-05-18 10-46-00.pngScreenshot from 2024-05-18 10-45-53.pngScreenshot from 2024-05-18 10-45-34.png

0 Kudos
Reply

1,109 Views
Alejandro_Salas
NXP TechSupport
NXP TechSupport

Hello @srinivas_123 

 

The image was generated successfully, you can see the file with extension .wic.zst.

 

You can decompress that file with zstd -d your_file.wic.zst command and you will have your pure wic file.

 

Best regards.

Salas.

0 Kudos
Reply

1,155 Views
srinivas_123
Contributor III

Screenshot from 2024-05-18 10-46-14.pngScreenshot from 2024-05-18 10-46-30.pngScreenshot from 2024-05-18 10-46-24.pngScreenshot from 2024-05-18 10-45-43.pngScreenshot from 2024-05-18 10-44-03.pngScreenshot from 2024-05-18 10-46-00.pngScreenshot from 2024-05-18 10-45-53.pngScreenshot from 2024-05-18 10-45-34.png

0 Kudos
Reply