imx how and where to set U-boot logging and kernel logging level after image build?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx how and where to set U-boot logging and kernel logging level after image build?

3,448 Views
munchiis
Contributor I

I would like to know where to set the logging level for both u-boot and kerne lbefore and after building the image 

I cant find where and how to change the loglevel and set it equal to 8.  

 

where and how do i set these for uboot? and is there an equivalent for the kernel logging

    CONFIG_LOG - Enables the logging system
    CONFIG_LOG_MAX_LEVEL - Max log level to build (anything higher is compiled out)
    CONFIG_LOG_CONSOLE - Enable writing log records to the console
0 Kudos
Reply
1 Reply

3,371 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Which platform are you using? https://developer.toradex.com/knowledge-base/splash-screen-linux Hope this can do some help for you.

0 Kudos
Reply