imx-hdmi-audio: HDMI Video is not ready!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx-hdmi-audio: HDMI Video is not ready!

Jump to solution
2,849 Views
adrianhill
Contributor I

I am trying to get started with a brand new SABRE i.MX6Quad board.

Using the Android distribution "out of the box" correctly boots, and displays Android on a regular HDMI monitor.

 

I then tried using the Linux distribution Linux 4.1.15_1.0.0 off the NXP page

IMX6_SW: i.MX 6 Series Software and Development Tool Resources

(without making any changes).

 

Booting off an SD card progresses until this message:

imx-hdmi-audio imx-hdmi-audio: ASoC: can't open platform imx-hdmi-audio: -22

imx-hdmi-audio imx-hdmi-audio: HDMI Video is not ready!

imx-hdmi-audio imx-hdmi-audio: ASoC: can't open platform imx-hdmi-audio: -22

imx-hdmi-audio imx-hdmi-audio: HDMI Video is not ready!

imx-hdmi-audio imx-hdmi-audio: ASoC: can't open platform imx-hdmi-audio: -22

imx-hdmi-audio imx-hdmi-audio: HDMI Video is not ready!

imx-hdmi-audio imx-hdmi-audio: ASoC: can't open platform imx-hdmi-audio: -22

imx-hdmi-audio imx-hdmi-audio: HDMI Video is not ready!

imx-hdmi-audio imx-hdmi-audio: ASoC: can't open platform imx-hdmi-audio: -22

imx-hdmi-audio imx-hdmi-audio: HDMI Video is not ready!

imx-hdmi-audio imx-hdmi-audio: ASoC: can't open platform imx-hdmi-audio: -22

imx-hdmi-audio imx-hdmi-audio: HDMI Video is not ready!

imx-hdmi-audio imx-hdmi-audio: ASoC: can't open platform imx-hdmi-audio: -22

imx-hdmi-audio imx-hdmi-audio: HDMI Video is not ready!

imx-hdmi-audio imx-hdmi-audio: ASoC: can't open platform imx-hdmi-audio: -22

 

What am I doing wrong? I expected that the "official" distribution would "just work".

The version number from the boot text is:

Freescale i.MX Release Distro 4.1.15-1.0.0 imx6qdlsolo

(the full text from the boot, captured on TeraTerm is attached.

I also tried the Linux 3.14.52 archived version off the same page, but got the same result.

I can log in from a TeraTerm instance on a PC.

 

Any help would be much appreciated!

Thanks

 

Original Attachment has been moved to: boot.txt.zip

Labels (2)
0 Kudos
1 Solution
1,064 Views
igorpadykov
NXP Employee
NXP Employee

Hi Adrian

hdmi should be set in kernel boot parameter, please refer to

attached Release Notes sect.4 Kernel Boot Parameters for  parameter

"video on 6SABRE-SD" and examples in Linux Guide sect.4.7 Running Linux OS

on the target, "Specifying displays", sect.4.7.1 Running Linux OS from MMC/SD

Best regards

igor
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
1,065 Views
igorpadykov
NXP Employee
NXP Employee

Hi Adrian

hdmi should be set in kernel boot parameter, please refer to

attached Release Notes sect.4 Kernel Boot Parameters for  parameter

"video on 6SABRE-SD" and examples in Linux Guide sect.4.7 Running Linux OS

on the target, "Specifying displays", sect.4.7.1 Running Linux OS from MMC/SD

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos