Hello,
I have a MCIMX8QM borad and 88W8997 module of SDIO interface.
If I flash linux image which is based on LF_v5.10_2.0.0 to MCIMX8QM and connect 88W8997 module, the wifi module works well.
When I tested based on Linux, I followed doccument UM11483.pdf.
By the way, I want to test on Android. It seems that Android only support PCIe interface.
I have two question.
1. Does SDIO interface support based on imx-android-10.0.0_2.6.0?
2. If question 1 is yes, how can I change to support SDIO interface?
Hardware: MCIMX8QM , 88W8997 module of Laird Company.
OS: imx-android-10.0.0_2.6.0
Thank you.
Solved! Go to Solution.
Hi Young
>1. Does SDIO interface support based on imx-android-10.0.0_2.6.0?
not sorry. One can try to use imx8qm-mek-usdhc3-m2.dts and follow UM11558 sect.4.3 Enabling uSD/M.2
Best regards
igor
Hi Young
>1. Does SDIO interface support based on imx-android-10.0.0_2.6.0?
not sorry. One can try to use imx8qm-mek-usdhc3-m2.dts and follow UM11558 sect.4.3 Enabling uSD/M.2
Best regards
igor