imx Krogoth Yocto patch /init.d/bluetooth help!

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx Krogoth Yocto patch /init.d/bluetooth help!

1,309 次查看
edwardtyrrell
Senior Contributor I

Hello,

I'm after a few instructions on how to apply a custom patch to /etc/init.d/bluetooth within one of my own custom meta-layers.

With other patches/file updates I've done it's simply a matter of coping a like mannered path to my own layer to that of the one I need to change - e.g update a pulseaudio file I'd do => meta-mylayer/recipes-multimedia/pulseaudio/etc, .  adding a bbappend and so. But how can I update /etc/init.d/bluetooth as it's not specifically in the sources/meta-....?

What would I have to include recipe wise inside my custom layer and how would the append work to apply a patch ( or replace the file out-right )?  

 Thanks. 

标签 (4)
0 项奖励
回复
2 回复数

1,033 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Edward Tyrrell,

Have you made progress on this regard?

There is a document which shows how to add a file, which you may use to replace the file altogether. You may then create a new image recipe or append on your new layer to include this recipe.

https://community.nxp.com/docs/DOC-105374

It is definitely not straightforward but I hope it helps!

Regards,

0 项奖励
回复

1,033 次查看
edwardtyrrell
Senior Contributor I

Hi,

Yes in the end I did.

Thanks.

0 项奖励
回复