imx_KK4.4.3_2.0.0-ga Over The Air (OTA) Question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx_KK4.4.3_2.0.0-ga Over The Air (OTA) Question

947 Views
sepljo
Contributor II

Hi all,

I've got a question regarding the generation of over the air images for android.

I've followed the steps outlined in the AOSP document to generate an OTA package. However, I'm not able to boot the device after the upgrade.

Some further info:

I'm using a EVK6SL board and have generated the images as follows:

source build/envsetup.sh && lunch evk_6sl-eng

make dist DIST_DIR=dist_output

./build/tools/releasetools/ota_from_target_files evk_6sl-target_files-{nnnn}.zip ota_update-{nnnn}.zip

However, after the upgrade, the new kernel fails to load at startup

U-Boot 2014.04-08637-gaffa032 (Apr 24 2015 - 11:53:05)

CPU:   Freescale i.MX6SL rev1.2 at 396 MHz

CPU:   Temperature 32 C, calibration data: 0x5895155f

Reset cause: POR

Board: MX6SLEVK

I2C:   ready

DRAM:  1 GiB

MMC:   FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2

*** Warning - bad CRC, using default environment

In:    serial

Out:   serial

Err:   serial

Found PFUZE100 deviceid=10,revid=11

Detecting VOL_DOWN+POWER key for recovery(0:0) ...

check_and_clean: reg 0, flag_set 0

Fastboot: Normal

flash target is MMC:1

Net:   FEC [PRIME]

Normal Boot

Hit any key to stop autoboot:  0

booti mmc1

kernel   @ 80808000 (6714592)

ramdisk  @ 81800000 (502095)

kernel cmdline:

        use boot.img command line:

        console=ttymxc0,115200 init=/init androidboot.console=ttymxc0 consoleblank=0 androidboot.hardware=freescale androidboot.serialno=213231d4dac8184b

switch to ldo_bypass mode!

Starting kernel ...

**** hangs here ****

Additionally, I've noticed that incremental updates fail to take effect due to partition // having an invalid checksum (output captured from the recovery log):

file "EMMC:/dev/block/mmcblk1p1:7221248:a27e8882206e834819a5435bc48c8a63040d7f51:7221248:0011fd17ac808f8e89da73471178ca767d370189" doesn't have any of expected sha1 sums; checking cache

failed to stat "/cache/saved.file": No such file or directory

Investigating further, I've noticed that the actual boot image included in the OTA package is different from the one that is used when downloading the image via mfgtool.

/myandroid/out/target/product/evk_6sl/boot-imx6sl.img (7258398)

ota boot.img (7221248)

It appears that the android OTA build tools use the raw kernel image to generate the boot image.

Is anyone able to point out what I need to do to generate valid OTA images? Has anyone else had any success with this?

Thanks

0 Kudos
Reply
3 Replies

656 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Joyce,

I’m afraid that OTA features are not supported, as they are not included on Freescale release BSPs.

Best regards!

/Carlos

0 Kudos
Reply

656 Views
chenguoyin
NXP Employee
NXP Employee

Please check the user guide in release package as "make otapackage" to build the ota package.

# Build images for i.MX6SoloX SABRE-AI board

$ source build/envsetup.sh

$ lunch sabreauto_6sx-user

$ make

$ make otapackage # you can generate ota package with this command.

0 Kudos
Reply

656 Views
jamesbone
NXP TechSupport
NXP TechSupport

I Think this package it is not included in our latest BSP, can you please clarify to the customer which version are you mention? 

0 Kudos
Reply