imx 6 Dual or Dual Plus evm

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx 6 Dual or Dual Plus evm

976 Views
jasonlambert
Contributor III

Hi Team,

Are there any EVMs out there for the IMX 6 Dual or Dual +? I'm only coming across designs for Quad. 

Jason 

Labels (2)
0 Kudos
Reply
1 Reply

887 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jason

you are right such nxp reference boards are not available, one can use Quad and use

kernel boot parameter maxcpus=n : n >= 0 limits the kernel to using 'n' processors.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply