HI ,
We are using MCIMX7 SABRE 700-28590 REV D . wHEN BOOTING USING THE 342-00659 REV B1 sdcard which is having 4.1.15_2.0.1 B version we are getting GUI image on HDMI display .But when tried to build image using imx-4.9.88-2.0.0_ga not getting GUI ON HDMI,getting embedded linux splash and progress bar ,but no GUI after that .Followed all the instructions as per latest bundled documents and read me.Also tried setting bootargs also.Please help to fix resolve this issue.
Thanks in advance .
sam
Please suggest a fix/solution for the issue . How to get HDMI working.
Thanks,
Syam
If you want to have QT GUI, you need to build the QT image. You can follow the Yocto User's guide to build the QT image.
Hi Jimmy,
Thanks for your reply.Iam not getting anything on my display after boot splash screen is going dark.Its like that after kernal loading also.
Is there any particular configuration or setting Iam missing.
Thanks,
Sam
Do you set the HDMI as a display in the bootargs?
For example:
Boot up the system through rootfs in eMMC, using HDMI as display.
For i.MX 7Dual SABRE boards :
U-Boot > setenv mmcargs 'setenv bootargs ${bootargs} root=/dev/mmcblk2p2 rootwait rw video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24'
For more information about bootargs setting, please read the i.MX_Linux_User's_Guide.pdf. You can download the BSP documentation from here: i.MX Software|NXP
Hi,
I tried bootargs already,without any success.
I can run display tests from unit tests,but startup display blank.
Thanks,
Syam,