imX23 LCD_PANEL=LMS430 how to initialise

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imX23 LCD_PANEL=LMS430 how to initialise

803 Views
Nagraj
Contributor I

As per the reference manual imx23 I have added the necessary functions in the boot_prep,init.c .

The sd card boot fails even though the build was successful? Can somebody help me in initiating this device using imx23 processor

Thanks in advance.

0 Kudos
2 Replies

538 Views
Nagraj
Contributor I
Thanks yaar, iam able to see while booting the functions called for the lcd_panel like lcdif_init(); init_timings(); backlight_init(); stmp3xxx_init_lcdif(); stmp3xxx_lcdif_dma_init(); stmp3xxx_lcdif_run(); are all called properly. Im unable to verify this with the hardware as there is some time for the hardware procurement! Mean while can you plz let me know what exactly is the procedure to initialse the 4.3" Lcd panel for imx233 processor??
0 Kudos

538 Views
Balaji_ng
Contributor III

Can you share the boot log messages?

Regards,

Balaji

0 Kudos