im8qxp single gpio pins to M4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

im8qxp single gpio pins to M4

481 Views
angelo_d
Senior Contributor I

Hi all,

my assumption is that only a full bank of gpio pins can be assigned to A or M4 side, not a single GPIO pin. Is this correct ?

Regards

angelo

 

0 Kudos
2 Replies

468 Views
kef2
Senior Contributor IV
  • what do you mean full bank of gpio pins? give me an example

gpio peripheral module includes bunch of IO pins, usually 32. It is easy to remove whole gpio "bank" from device tree on Linux and use it exclusively on M4. Easy to say, hard to do since it puts serious limits on pin usage. It is big problem NXP should address. 

@angelo_d, yes it is "easier" to dedicate whole bank to M4. There's semi-complete driver drivers/gpio/gpio-imx-rpmsg.c, which was introduced in imx7ulp BSP. It is supposed to run on Linux, and corresponding SRTM service is supposed to run on M4. Unfortunately semi-, because it had GPIO interrupts and usage from atomic kernel context incomplete. Perhaps it has changed, I don't know. See attached driver with my mods, which seems working well on imx7d. For SRTM code please look in imx7ulp BSP.

 

0 Kudos

472 Views
joanxie
NXP TechSupport
NXP TechSupport

what do you mean full bank of gpio pins? give me an example

0 Kudos