im6q如何制作属于自己硬件的mfgtools的firmware

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

im6q如何制作属于自己硬件的mfgtools的firmware

1,996 Views
wangzhiqiang
Contributor I

我用的是自己的im6q硬件板,烧录下载时总是卡在jump to os image。而且串口无输出任何信息。我用的是android4.4.2的bsp包

所以我想我需要修改mfgtools的OS Firmware里的uboot.bin和uimage。在论坛里有看到有人讨论关于编译自己的firmware的方法,但我在freescale的官网找不到下载的代码。

请问我如何获取编译mfgtools的os firmware的代码,以及如何编译属于自己的firmware。

Labels (5)
0 Kudos
Reply
1 Reply

1,021 Views
BiyongSUN
NXP Employee
NXP Employee

Freescale_Yocto_Project_User's_Guide

6.2 The Manufacturing Tool, MFGTool

One way to place an image on a device is to use the Manufacturing Tool, MFGTool. The recipes used to build a

manufacturing tool image are linux-imx-mfgtool and u-boot-mfgtool.

To build a manufacturing image do the following -

$ bitbake fsl-image-mfgtool-initramfs

A manufacturing tool kernel is built using the imx_v7_mfg_defconfig while the default kernel is built by using the

imx_v7_defconfig. This is handled automatically by the MFGTool recipes listed above.

For more details on how to use the manufacturing tool, see Section "How to Enter Serial Download Mode for MFGTool" in

the i.MX Linux User's Guide.

0 Kudos
Reply