if imx27 support WinCE 2013?
Hi, I 'd like to check that if imx27 support WinCE 2013?
I use it for WinCE6 and update it to WinCE7 in last years.
But you know, WinCE 7 is going out of support. So I need do an update or change.
There are lots of devices already sailed and on market. So I only want to do a SW update. No HW update for easy service.
So is there a way to support WinCE2013 on imx27?
Thanks.
Hi,
Thanks for your feed back.
Do you mean NXP/ Freescale are working on the WinCE2013 for iMX27?
And is there a timeline for that?
I mean that the WinCE2013 has been come out for 6 years.
I can understand that iMX27 is too old or slow for Wince2013.
So if there will not be a update package for iMX27 is understandable.
Please just let me know if there is a update for this.
Thanks.
Hello Kevin,
Sorry, Unfortunately Wince 2013 is not done for MX27, there is not much effort in MX27 since it will end soon.
Regards
Hi,
Thanks for your feed back.
Do you mean NXP/ Freescale are working on the WinCE2013 for iMX27?
And is there a timeline for that?
I mean that the WinCE2013 has been come out for 6 years.
I can understand that iMX27 is too old or slow for Wince2013.
So if there will not be a update package for iMX27 is understandable.
Please just let me know if there is a update for this.
Thanks.