if I want to add/delete qt assembly such as linuxfb, what should I do?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

if I want to add/delete qt assembly such as linuxfb, what should I do?

1,308件の閲覧回数
cilymo
Contributor I

if I want to add/delete qt assembly such as linuxfb, what should I do?

My BSP is 4.1.15.

ラベル(2)
0 件の賞賛
返信
1 返信

1,249件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi cily

please refer to fsl-image-qt5 in Table 1. Freescale Yocto project images attached Yocto Guide

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信