iW-RainboW-G15M boot from SD card on Linux pc

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iW-RainboW-G15M boot from SD card on Linux pc

502 Views
raghavendrasurp
Contributor II

Hi All,

We are using iW-RainboW-G15M, initial we have checked board boot from SPI nor flash, but we want to do custom boot from SD card , So how to do without using MFG tool on linux PC, Please give me any solution

Thanks

Raghavendra

0 Kudos
Reply
1 Reply

451 Views
igorpadykov
NXP Employee
NXP Employee

Hi Raghavendra 

one can follow guidelines provided in Linux Gudie from NXP Linux documentation

page

i.MX Software|NXP 

However specific for that module documentation may be obtained from vendor resources

i.MX6 Qseven SOM Module | iWave Systems 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply