iMxRT1021 hardfault in IAR C++ library

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMxRT1021 hardfault in IAR C++ library

1,148件の閲覧回数
ChengGu
Contributor I

To whom it may concern,

 I am using iMxRT1021 dev board, my IDE is IAR, my project use many C++ object such as map etc. sometime, my code get hardfault while running in these IAR C++ library codes, or my map objects are crashed in the middle. could this relate with iMxRT cache setting? any suggestion on how to debug such issue? thanks a lot.

Best

Gu

ラベル(2)
0 件の賞賛
返信
1 返信

1,134件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Firstly, I'd like to know whether you locate the code line that invokes the hardfault interrupt. next, I was wondering if you can introduce these C++ libraries briefly.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信