iMx8mq lpddr4 flash.bin

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMx8mq lpddr4 flash.bin

1,385 次查看
1316244577
Contributor II

HI all:

This error occurred while compiling flash.bin for my own board

pastedImage_1.png
I passed both the DDR calibration and the stress test then generate the lpddr4 times.c file

I copied the file as required by i.MX Linux® User's Guide5.13

Is this error missing u-boot.itb?

Where does the u-boot.itb file come from?

标记 (1)
0 项奖励
回复
1 回复

1,239 次查看
igorpadykov
NXP Employee
NXP Employee

Hi

for new memory one can follow Chapter 4 How to bring up a new MX8MSCALE board
p.13 MSCALE_DDR_Tool_User_Guide.pdf included in

i.MX8 MSCALE SERIES DDR Tool Release (V2.10) 

also detailed build steps can be found on

https://developer.solid-run.com/knowledge-base/i-mx8m-atf-u-boot-and-linux-kernel/ 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复