iMx8M Plus how to boot from QSPI NOR Flash

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMx8M Plus how to boot from QSPI NOR Flash

1,355 次查看
KLuis
Contributor I

Hi,

Referring to Table 6-32 in the i.MX 8M Plus Applications Processor Reference Manual, it looks like there is no boot device for QSPI NOR flash using FlexSPI. I can find NOR flash boot select using Hyperflash or eCSPI. What settings are required to boot from QSPI NOR flash?

0 项奖励
回复
3 回复数

1,327 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Rita_Wang_0-1718684978318.png

And our reference design The QSPI memory is connected to the FlexSPI interface of i.MX 8M PluS

0 项奖励
回复

1,315 次查看
KLuis
Contributor I

Hi Rita,

The table is the same as the Table 6-32. Your reply does not provide further details for booting from QSPI NOR Flash. In addition, some posts mention about using "FlexSPI 3B" to boot QSPI NOR Flash. Is there any info about "FlexSPI 3B" and how to use this mode to boot QSPI NOR Flash?

0 项奖励
回复

1,196 次查看
KLuis
Contributor I

The choice of QSPI NOR Flash has 3/4-byte addressing options. The booting option is set to “FlexSPI 3B”. The system will boot from the NOR Flash using 3-byte addressing.

0 项奖励
回复