iMx7D HAB Event issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMx7D HAB Event issue

Jump to solution
4,439 Views
bobbychen197805
Contributor II

I test the HAB boot on SPI-Flash on imx7d and get a HAB event as follows, can anyone tell me what it's means?

=> hab_status

Secure boot disabled

HAB Configuration: 0xf0, HAB State: 0x66

--------- HAB Event 1 -----------------
event data:
0xdb 0x00 0x14 0x42 0x33 0x22 0x33 0x00
0x00 0x00 0x00 0x0f 0x00 0x91 0x10 0x00
0x10 0x00 0x00 0x00

STS = HAB_FAILURE (0x33)
RSN = HAB_INV_ADDRESS (0x22)
CTX = HAB_CTX_TARGET (0x33)
ENG = HAB_ENG_ANY (0x00)

Based on the Comment in hab.h, this event logged in hab_rvt.check_target().

Reference to “3.3 Check Target” of “HAB4_API.pdf”:

  hab_status_t(* hab_rvt::check_target)(hab_target_t type, const void *start, size_t bytes)

I guess the parameters are: type -> 0x0f, *start -> 0x00911000, bytes -> 0x10000000 ?? Correct??

If it is correct, the size (0x10000000??) seems unreasonable.

Any suggestions?

Labels (2)
0 Kudos
Reply
1 Solution
4,301 Views
Yuri
NXP Employee
NXP Employee

Hello,

 I've sent You some comments directly.

Regards,

Yuri.

View solution in original post

8 Replies
4,301 Views
matias_larsson
Contributor II

Hi Bobby,

We have the exact same problem with our i.MX7D, please check my thread https://community.nxp.com/thread/512577 . When I change the load address to DRAM, it works. Right now I don't have access to the CSF but I can say with confidence that the authenticated region length was the same regardless of load address. I will anyway verify my CSF once I get back and then reply to my own thread accordingly.

BR

Matias Larsson

0 Kudos
Reply
4,301 Views
bobbychen197805
Contributor II

Yes, but it only occurs on boot from SPI-Flash. It works fine on boot from mmc.

0 Kudos
Reply
4,302 Views
Yuri
NXP Employee
NXP Employee

Hello,

 I've sent You some comments directly.

Regards,

Yuri.

2,189 Views
narkoskatona
Contributor II

I have a similar problem



HAB Configuration: 0xf0, HAB State: 0x66

--------- HAB Event 1 -----------------
event data:
0xdb 0x00 0x14 0x42 0x33 0x22 0x33 0x00
0x00 0x00 0x00 0x0f 0x00 0x90 0x70 0x00
0x00 0x01 0x12 0x00

STS = HAB_FAILURE (0x33)
RSN = HAB_INV_ADDRESS (0x22)
CTX = HAB_CTX_TARGET (0x33)
ENG = HAB_ENG_ANY (0x00)


--------- HAB Event 2 -----------------
event data:
0xdb 0x00 0x14 0x42 0x33 0x22 0x33 0x00
0x00 0x00 0x00 0x0f 0x00 0x90 0x70 0x00
0x00 0x01 0x10 0x60

STS = HAB_FAILURE (0x33)
RSN = HAB_INV_ADDRESS (0x22)
CTX = HAB_CTX_TARGET (0x33)
ENG = HAB_ENG_ANY (0x00)



could you please, ad some more details?

0 Kudos
Reply
3,183 Views
pirors
Contributor I

Hi @Yuri  , can you please tell me the solution? I have a similar problem on i.MX6UL:
https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-Secureboot-SPL-Verification/td-p/1760513

Thanks

0 Kudos
Reply
4,301 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Length of 0x10000000 bytes means 256 MBytes - this is bigger that size of the OCRAM, but 

for DRAM it looks as workable. 

Regards,

Yuri.

0 Kudos
Reply
4,301 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

   Yes, the size of 0x10000000 is very big for OCRAM.    

Have a great day,

Yuri

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos
Reply
4,301 Views
bobbychen197805
Contributor II

Yes, but why? It looks like the behavior of bootrom. How to debug?

0 Kudos
Reply