iMx6UL supply voltage dip

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMx6UL supply voltage dip

533 Views
prasadgj
Contributor II

HI,

In our design, we have voltage monitoring with watchdog(max16002) for processor voltages(5V, 3.3V, VDDARM, VDDR1V5), this voltages are generated by LDOs.  In voltage monitoring watchdog any voltage dip means watchdog has to trigger. 

is their any way in processor that voltage level can be made dip so that watchdog can be tested?.

one way is hardware voltage injecting to input of voltage monitoring ICs but we are looking in software level that in processor can be loaded so that voltages levels are dip.

0 Kudos
Reply
2 Replies

467 Views
prasadgj
Contributor II

Hi Igor,

Whether can we find any technical reference/calculation to do high loading processor(timing of video) to dip some voltage level. 

we are tried to play some 15min of video file and monitor the voltage, I didn't find any dip in voltage.

0 Kudos
Reply

467 Views
igorpadykov
NXP Employee
NXP Employee

Hi Prasad

unfortunately from processor side there are no ways to make

that voltage levels can be dip. In general one can attach resistor with low

value and try to toggle it from software. High loading processor (like running video)

also may lower processor voltages.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply