iMXRT1172 SNVS bank -ON/OFF pin function query

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMXRT1172 SNVS bank -ON/OFF pin function query

ソリューションへジャンプ
1,139件の閲覧回数
vihang_vinayak
Contributor II

Hi,

We are using the iMXRT1172 in one of the battery application project. In my project to put iMXRT1172 in SNVS mode we are using the ONOFF pin (Ball no: U10) 

We just want to know if the ONOFF pin is independent of the execution code incase if the firmware gets stuck internally. I should be able to use the functionality of emergency off using the ONOFF pin.

Please confirm that the ONOFF pin is independent of the execution of code.

Quick response is appreciated.

Best Regards,

Vihang Waze

Design Engineer

Tata Elxsi Limited

0 件の賞賛
返信
1 解決策
1,120件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Yes, the ONOFF pin is independent of the execution of code.

 

BR,

Edwin.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,117件の閲覧回数
vihang_vinayak
Contributor II

Thank you Edwin for the confirmation

0 件の賞賛
返信
1,121件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Yes, the ONOFF pin is independent of the execution of code.

 

BR,

Edwin.

0 件の賞賛
返信