iMXRT-1064; booting directly to active firmware in internal FLASH

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMXRT-1064; booting directly to active firmware in internal FLASH

Jump to solution
1,023 Views
jaripeltonen
Contributor IV

Hello!

I'm working on a project where we use iMXRT-1064. I have a question regarding Firmware swap feature that is introduced in document AN12255 and AN12240. This question is also linked to discussion thread on the same topic (https://community.nxp.com/t5/i-MX-RT/iMXRT1064-Issue-with-firmware-swap/m-p/1345041#M16437)

The question is; Is it possible to set iMXRT-1064 to automatically boot directly to a predefined (active) FLASH section, so that the API function call "bl_firmware_switch()" would not be needed?

An example; the internal FLASH is divided into two 2 MByte sections (0 and 1), and the active (latest) firmware has been programmed into section 1 (address 0x7020 0000). Now, the device boots up on section 0 (0x7000 0000) and from there we have to jump to section 1 in order to run the latest SW image. Is there any way to make the processor to boot directly from section 1 so that the jump command would not be needed?

Thanks & best regards,

Jari

Labels (1)
0 Kudos
Reply
1 Solution
1,014 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is it possible to set iMXRT-1064 to automatically boot directly to a predefined (active) FLASH section, so that the API function call "bl_firmware_switch()" would not be needed?
-- No, I'm afraid not
Have a great day.
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,015 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is it possible to set iMXRT-1064 to automatically boot directly to a predefined (active) FLASH section, so that the API function call "bl_firmware_switch()" would not be needed?
-- No, I'm afraid not
Have a great day.
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
1,009 Views
jaripeltonen
Contributor IV

Hi Jeremy,

Thanks for your fast reply!

I will close this thread as I have no further questions.

Best regards,

Jari

0 Kudos
Reply