iMX93 use CSI Pattern Generator error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX93 use CSI Pattern Generator error

524 Views
ranYang
Contributor III

hello:

      I use iMX93 evk lf6.12.20-gdfaf2136deb2 version, I use command 

v4l2-ctl -d /dev/v4l-subdev2 --set-ctrl=test_pattern=1  test ,and use 

media-ctl -d /dev/media0 -l "'ar0521 2-0036':0 -> 'csidev-4ae00000.csi':0 [1]"
media-ctl -V "'ar0521 2-0036':0 [fmt:BGR888_1X24/2592x1944 field:none colorspace:raw]"
media-ctl -V "'csidev-4ae00000.csi':0 [fmt:BGR888_1X24/2592x1944 field:none colorspace:raw]"
media-ctl -V "'csidev-4ae00000.csi':1 [fmt:BGR888_1X24/2592x1944 field:none colorspace:raw]"
media-ctl -V "'crossbar':0 [fmt:BGR888_1X24/2592x1944 field:none colorspace:raw]"
media-ctl -V "'crossbar':2 [fmt:BGR888_1X24/2592x1944 field:none colorspace:raw]"
media-ctl -V '"mxc_isi.0":0 [fmt:BGR888_1X24/2592x1944 field:none colorspace:raw]'
media-ctl -V '"mxc_isi.0":1 [fmt:BGR888_1X24/2592x1944 field:none colorspace:raw]'

and use 

v4l2-ctl -d /dev/video0 --set-fmt-video=width=2592,height=1944,pixelformat=RGB3 --stream-mmap --stream-count=1  Collect video streams  and is block. The attachment is log print, thank you.

卡死.PNG

 

 

0 Kudos
Reply
2 Replies

505 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

 

Per your log it looke like the ar0521 does not support the format you are try to evaluate, please check it.

Regards

0 Kudos
Reply

497 Views
ranYang
Contributor III

hello:

       Without sensor access, test the driver file interface for simulating CSI data streams

0 Kudos
Reply