iMX93 linux prebuilt image and flashing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX93 linux prebuilt image and flashing

ソリューションへジャンプ
4,479件の閲覧回数
KHL
Contributor I

Hi,

I dowloaded iMX93 evk prebuilt images "LF_v6.1.1_1.0.0_images_IMX93EVK", there are lots of dtb, bin files in the package. I wish to flash back the default images, which image should I flash and how ?

I tried using uuu to flash "imx-image-full-imx93evk.tar.zst", but an error pops up as per below 

KHL_1-1685623336248.png

I tried switch to using a linux host machine, the uuu outcome remains. What went wrong ?

Thanks.

 

0 件の賞賛
返信
1 解決策
4,464件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

I hope you are doing well.

I suggest you use the next command with the board on USB serial download mode.

uuu -b emmc_all imx-image-full-imx93evk.wic

Best regards.

Jorge.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
4,465件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

I hope you are doing well.

I suggest you use the next command with the board on USB serial download mode.

uuu -b emmc_all imx-image-full-imx93evk.wic

Best regards.

Jorge.

0 件の賞賛
返信
4,451件の閲覧回数
KHL
Contributor I

Thank you. It works.

0 件の賞賛
返信