iMX93 USB 2.0 device tree node undefined

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX93 USB 2.0 device tree node undefined

272 Views
AlanWen
Contributor III

I'm using the iMX93 EVK board porting USB 2.0 device tree, the original source code is porting fort type-C.
I'd tried to post the code below in u-boot dts (imx93-11x11-evk.dts) but it doesn't work.

reg_usb0_host_vbus: regulator-usb0-vbus {
		compatible = "regulator-fixed";
		regulator-name = "usb0_host_vbus";
		regulator-min-microvolt = <5000000>;
		regulator-max-microvolt = <5000000>;
		enable-active-high;
		regulator-always-on;
	};

 

Also, I tried to modify the usb node for switching to host mode as below. It seems not a correct way to port USB as host.

&usbotg1 {
	dr_mode = "host";
	status = "okay";
};

 

And then modifying the configuration in imx93-11x11_evk_defconfig.

# CONFIG_USB_TCPC is not set
CONFIG_IMX_HAB=y


How can I modify the code for USB 2.0 ?
Could you please provide a complete sample code

 

Thanks

0 Kudos
Reply
1 Reply

244 Views
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

According to Reference Manual p. 90 you should make it with dr_mode change made. Could you try to remove the config:

 

[*] ChipIdea device controller

 

Or is this issue only persistent in u-boot?

Also, is your work over an EVK or custom board? i.MX 93 processor has USB 2.0 already,

Regards

0 Kudos
Reply