[iMX93] ADC calibration failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[iMX93] ADC calibration failed

1,132件の閲覧回数
charleshuang
Senior Contributor II

Hi NXP Team,

I just enable 'adc1' in our device tree, but the system reponse the calibration failed.

What could be the reason?

 

&adc1 {
vref-supply = <&reg_vref_1v8>;
status = "okay";
};

 

root@imx93afee320a1:/sys/bus/iio/devices# dmesg| grep adc
[ 1.565952] Bluetooth: HCI UART protocol Broadcom registered
[ 1.719162] imx93-adc 44530000.adc: ADC calibration failed!
[ 1.724775] imx93-adc: probe of 44530000.adc failed with error -11
[ 1.842125] can: broadcast manager protocol

 

タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,121件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Which version BSP are you using? Are you using the NXP 93EVK BOARD?

0 件の賞賛
返信

889件の閲覧回数
RainChou
Contributor I

Hello, NXP team. I have encountered the same issue. My IMX93 ADC also shows the errors 'imx93-adc 44530000.adc: ADC calibration failed!' and 'imx93-adc: probe of 44530000.adc failed with error -11' during initialization. I am using Advantech's IMX93ROM-2820A1 core board.

0 件の賞賛
返信