iMX8mp gpio configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8mp gpio configuration

Jump to solution
12,426 Views
mukesh_kumar
Contributor III

hello

could you please help me out to configure GPIO1_IO6  with internal PULLUP . below are the DTB contents i found relevant to the GPIO configuration which i'll be using in my driver.

By default we are getting line in pulled LOW state now. we need to configure in pulled high state by default. 

https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mp-pinfu... 

/*
* The pin function ID is a tuple of
* <mux_reg conf_reg input_reg mux_mode input_val>
*/

#define MX8MP_IOMUXC_GPIO1_IO06__GPIO1_IO06   0x02C 0x28C 0x000 0x0 0x0

 

https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mp-evk.d...

&iomuxc {
              pinctrl_csi0_rst: csi0_rst_grp {
                              fsl,pins = <
                                             MX8MP_IOMUXC_GPIO1_IO06__GPIO1_IO06  0x19
                                              >;
            };
};

to my understanding the value 0x19 is writing to the below control register which is setting the GPIO to use as PULLDOWN.
where bit no:8 =0 and bit no:6=0.

Screenshot from 2021-09-03 20-20-57.png

 

is this the right approch, please help me understand it correctly.

Thanks in advance 

0 Kudos
Reply
1 Solution
12,416 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mukesh

 

> my understanding the value 0x19 is writing to the below control register which is

>setting the GPIO to use as PULLDOWN. where bit no:8 =0 and bit no:6=0.

 

for enabling pull resistor set bit no:8 =1

enable pull down(LOW)  bit no:6=0

enable pull up(HIGH)      bit no:6=1

 

Best regards
igor

View solution in original post

0 Kudos
Reply
4 Replies
12,396 Views
mukesh_kumar
Contributor III

Hi igor,

Thank you for replying to the issue.

I changed the value as 1 at bit number 6 and bit number 8 , but it seems not taking any effect to change as internal pullup
&iomuxc {
              pinctrl_csi0_rst: csi0_rst_grp {
                              fsl,pins = <
                                             MX8MP_IOMUXC_GPIO1_IO06__GPIO1_IO06  0x159
                                              >;
            };
};
for confirmation I tried reading register address 0x3033028C using devmem2, but it thrown a error mentioning bad address.

can you please answer the following queries
1.Does the control register I'm referring to is correct?
2.what is the correct physical address of the register that refer the preprocessor directive MX8MP_IOMUXC_GPIO1_IO06__GPIO1_IO06 ?
3.At the defination of this preprocessor directive the tuple contains a member named input_val, is it input to mux_reg or conf_reg ?
/* <mux_reg conf_reg input_reg mux_mode input_val>
*/

#define MX8MP_IOMUXC_GPIO1_IO06__GPIO1_IO06 0x02C 0x28C 0x000 0x0 0x0

can you please answer these queries,

Thank you,
Mukesh kumar

0 Kudos
Reply
12,390 Views
igorpadykov
NXP Employee
NXP Employee

devmem2 is not supported by nxp, please try memtool

https://source.codeaurora.org/external/imx/imx-test/tree/test/memtool?h=lf-5.10.y_2.0.0

 

Best regards
igor

0 Kudos
Reply
12,382 Views
mukesh_kumar
Contributor III

Hi igor,

I'm able to see that register contents are updating properly,
i also changed the drive strength field as well from X1 to X6 that helped to drive the pullup to 1.8V for me.

while the drive strength field is set X1 the pullup is able to drive 0.5V only.

thanks for the help.

12,417 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mukesh

 

> my understanding the value 0x19 is writing to the below control register which is

>setting the GPIO to use as PULLDOWN. where bit no:8 =0 and bit no:6=0.

 

for enabling pull resistor set bit no:8 =1

enable pull down(LOW)  bit no:6=0

enable pull up(HIGH)      bit no:6=1

 

Best regards
igor

0 Kudos
Reply