iMX8mm lpddr4 ROM table location Yocto zeus

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX8mm lpddr4 ROM table location Yocto zeus

1,129 次查看
mitchdz
Contributor I

Hello.

I am looking to enable secureboot in the Yocto zeus branch for iMX8mm.

I am using the following repo link to initialize the repository:

repo init -u https://source.codeaurora.org/external/imx/imx-manifest  -b imx-linux-zeus -m imx-5.4.3-2.0.0.xml

 

In order to use coresight, I need the Embedded Trace Macrocell (ETM) for each core defined in a devicetree, but can not find the address for this board. If I can get the location of the ROM table then I can find the offset for each core (see https://developer.arm.com/documentation/ddi0500/d/debug/rom-table/rom-table-register-summary).

 

This post is requesting the address of said ROM table, or the devicetree file to enable coresight components.

 

Thanks,

-Mitch

标签 (1)
标记 (3)
0 项奖励
回复
1 回复

1,117 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Mitch

 

one can look at suggestions provided on

https://community.nxp.com/t5/i-MX-Processors/openocd-imx8-coresight-address-help/m-p/608904

 

Best regards
igor

0 项奖励
回复