Dear support,
Could you clarify which compilation options are required to generate SCFW (as describer in imx_scfw_porting_kit_1.2.2), to match scfw-tcm.bin as fetched from NXP during Yocto build ?
Currently we face different behaviour during linux start on IMX8QXPMEK board:
A/ With default scfw-tcm.bin file (as fetched June 11th through YOCTO):
linux boot success (tycally can run graphic demos).
B/ with regenerated scfw-bin from imx_scfw_porting_kit_1.2.2 package:
linux boot failed during starup, complaining about access to graphic resources
I can provide you with detailed serial traces on both UART0 and M4 UART.
best regards,
Laurent