iMX8X MIPI DSI Burst mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX8X MIPI DSI Burst mode

1,527 次查看
emanuele79
Contributor III

I'm using IMX8X DSI output with Lontium lt8912. Lontium do not support burst mode, and the mainline driver do not set the relevant flag (correctly) when he call mipi_dsi_attach function.

But HDMI output (from Lontium) works only if I set burst mode on the iMX8X DSI output and this sounds strange.

Is there the possibility that the VIDEO_MODE register definition on iMX8X datasheet is not correct?

Thank you.

Emanuele

标记 (1)
0 项奖励
回复
2 回复数

1,502 次查看
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @emanuele79,

I hope you are doing well.

->The possibility that the VIDEO_MODE register definition on the iMX8X datasheet is not correct is low.

->Please make sure to check with different DMI/DSI output devices it may be problematic.
->Please make sure to check using different versions of the driver/ kernel version, which is recommended as it offers the latest driver/fw to use.

It may be helpful.

Thanks & Regards,
Sanket Parekh

0 项奖励
回复

1,003 次查看
arturobuzarra
Contributor III

Hi @Sanket_Parekh ,

We are facing a similar issue than reported by @emanuele79 with i.MX8QXP and Lontium LT8912B MIPI-DSI to HDMI bridge using your latest BSP "lf-6.6.36-2.1.0".

We are using the upstream driver from drivers/gpu/drm/bridge/lontium-lt8912b.c and according to the Lontium datasheet, LT8912B supports only Non-Burst mode video operation with Sync Events and continuous clock on clock lane. The i.MX8QXP platform does not work using the default Non-Burst mode with Sync Events however forcing to use the Burst mode it is working fine.

We already tested the same upstream driver with the default Non-Burst mode video operation with Sync Events on a i.MX93 and works fine, so it points that there is something wrong with the MIPI-DSI driver that uses the i.MX8QXP platform, "Northwest Logic MIPI DSI Host controller" (CONFIG_DRM_NWL_MIPI_DSI) located in drivers/gpu/drm/bridge/nwl-dsi.c.

Could you help to us to identify the root cause of that issue?

Thanks in advance,

Arturo.

0 项奖励
回复