iMX8ULP always-on 1hz refresh rate display example of AN13914

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX8ULP always-on 1hz refresh rate display example of AN13914

跳至解决方案
1,597 次查看
ferringer1
Contributor IV

Hello Community,

we do have an iMX8ULP evaluation board with the corresponding LCD display. While the display itself works fine under Linux, we are not able to the the 1Hz always-on display example from AN13914 running. Everything seems to work (we can reproduce the power consumption numbers etc), but the screen stays just black. We don't see any activity on the screen whatsoever.

Has anyone been able to get this demo running?

Regards,

Markus

0 项奖励
回复
1 解答
1,550 次查看
ferringer1
Contributor IV

As it turns out, there are two binary files in the ZIP file: 
flash_aod_RK055AHD091.bin
flash_aod_RK055MHD091.bin

*NOT* according to the description of the AN, you have to flash the second one, with the "M" in it. Works now.

Is there any chance to get the sourcecode of the M33 binaries? I cannot find it in the examples of the SDK.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,561 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @ferringer1 

 

Please check the steps refering the AN.

 

Best Regards

Zhiming

0 项奖励
回复
1,551 次查看
ferringer1
Contributor IV

As it turns out, there are two binary files in the ZIP file: 
flash_aod_RK055AHD091.bin
flash_aod_RK055MHD091.bin

*NOT* according to the description of the AN, you have to flash the second one, with the "M" in it. Works now.

Is there any chance to get the sourcecode of the M33 binaries? I cannot find it in the examples of the SDK.

0 项奖励
回复
1,503 次查看
bernhardfink
NXP Employee
NXP Employee

Hi Markus,

isn't it more or less this one:  ..\SDK_2_15_000_EVK-MIMX8ULP\boards\evkmimx8ulp\demo_apps\low_power_display

This is of course just the M33 part of it, the much bigger binaries from the app note software package also include the rest of the boot image.

 

Regards,
Bernhard.

标记 (2)
0 项奖励
回复