iMX8QXP-falied to on LVDS-HDMI display

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8QXP-falied to on LVDS-HDMI display

3,175 Views
kinjalGediya
Contributor III

Hi NXP,
We are using custom board of iMX8QXP-mek. We are using lvds in it and and we are not able start HDMI disaply.
There is only 1 port of LVDS in custom board which is LVDS0
We removed I/O expander in custom board and give 1.8V externally to MIPI_DSI0_EN pin, remaining things are same like clock and data pins.
We are getting PWM signal in mini SAS daughter board.
Another problem is we are not able to get clock on MIPI_DSI0_I2C0_SCL pin.
Can you please guide us for above issue?

0 Kudos
Reply
3 Replies

3,169 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
Reply

3,150 Views
kinjalGediya
Contributor III

Hello igor,

Thank you to your quick reply.


I resolve problem of I2C clock for lvds but getting error "it6263 19-004c: Probe failed. Remote port 'lvds-channel@0' disabled" and "it6263 20-004c: Probe failed. Remote port 'lvds-channel@0' disabled."

In custom board there is a direct 5v given to LVDS enable pin.

I also make changes in LVDS driver and in device tree.
Can you please guide us for above error?

U-Boot 2020.04-5.4.24-2.1.0+g4979a99 (Sep 25 2020 - 08:34:02 +0000)

CPU: NXP i.MX8QXP RevC A35 at 1200 MHz at 27C

Model: NXP i.MX8QXP MEK
Board: iMX8QXP ISSI-OSPI

BuildInfo:
- SCFW 4a1654e0, SECO-FW 376e3c15, IMX-MKIMAGE 6745ccdc, ATF 413e93e
- U-Boot 2020.04-5.4.24-2.1.0+g4979a99

Boot: MMC0
DRAM: 1022 MiB
setup_typec lookup GPIO5_9 failed ret = 3
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... *** Warning - bad CRC, using default environment

[*]-Video Link 0probe device is failed, ret 3
(1280 x 720)
[0] dpu@56180000, video
[1] lvds-channel@0, display
[2] lvds-to-hdmi-bridge@4c, video_bridge
In: serial
Out: serial
Err: serial
switch to partitions #0, OK
mmc0(part 0) is current device
flash target is MMC:0
Net: Could not get PHY for FEC0: addr 0
Could not get PHY for FEC0: addr 0
Could not get PHY for FEC1: addr 0
Could not get PHY for FEC1: addr 0
No ethernet found.

Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0(part 0) is current device
24470016 bytes read in 124 ms (188.2 MiB/s)
Booting from mmc ...
98818 bytes read in 11 ms (8.6 MiB/s)
## Flattened Device Tree blob at 83000000
Booting using the fdt blob at 0x83000000
Using Device Tree in place at 0000000083000000, end 000000008301b201
Disable clock-controller@5a4d0000 rsrc 62 not owned
Disable clock-controller@5ac90000 rsrc 102 not owned

Starting kernel ...

[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd042]
[ 0.000000] Linux version 5.4.24-2.1.0+ (oe-user@oe-host) (gcc version 9.2.0 (GCC)) #1 SMP PREEMPT Tue Sep 29 04:45:32 UTC 2020
[ 0.000000] Machine model: Freescale i.MX8QXP MEK
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] OF: reserved mem: failed to allocate memory for node 'linux,cma'
[ 0.000000] Reserved memory: created DMA memory pool at 0x0000000090000000, size 0 MiB
[ 0.000000] OF: reserved mem: initialized node vdev0vring0@90000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x0000000090008000, size 0 MiB
[ 0.000000] OF: reserved mem: initialized node vdev0vring1@90008000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x0000000090010000, size 0 MiB
[ 0.000000] OF: reserved mem: initialized node vdev1vring0@90010000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x0000000090018000, size 0 MiB
[ 0.000000] OF: reserved mem: initialized node vdev1vring1@90018000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x0000000090400000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vdevbuffer, compatible id shared-dma-pool
[ 0.000000] cma: Reserved 320 MiB at 0x00000000ac000000
[ 0.000000] earlycon: lpuart32 at MMIO 0x000000005a060000 (options '')
[ 0.000000] printk: bootconsole [lpuart32] enabled
[ 0.000000] NUMA: No NUMA configuration found
[ 0.000000] NUMA: Faking a node at [mem 0x0000000080200000-0x00000000bfffffff]
[ 0.000000] NUMA: NODE_DATA [mem 0xabdf6500-0xabdf7fff]
[ 0.000000] Zone ranges:
[ 0.000000] DMA32 [mem 0x0000000080200000-0x00000000bfffffff]
[ 0.000000] Normal empty
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000080200000-0x0000000083ffffff]
[ 0.000000] node 0: [mem 0x0000000086200000-0x0000000087ffffff]
[ 0.000000] node 0: [mem 0x0000000090020000-0x00000000901fffff]
[ 0.000000] node 0: [mem 0x0000000090500000-0x0000000091ffffff]
[ 0.000000] node 0: [mem 0x0000000094c00000-0x00000000bfffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000080200000-0x00000000bfffffff]
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: MIGRATE_INFO_TYPE not supported.
[ 0.000000] psci: SMC Calling Convention v1.1
[ 0.000000] percpu: Embedded 24 pages/cpu s58904 r8192 d31208 u98304
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] CPU features: detected: GIC system register CPU interface
[ 0.000000] Speculative Store Bypass Disable mitigation not required
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 204844
[ 0.000000] Policy zone: DMA32
[ 0.000000] Kernel command line: console=ttyLP0,115200 earlycon root=/dev/mmcblk0p2 rootwait rw
[ 0.000000] Dentry cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 7, 524288 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] Memory: 459276K/832384K available (14460K kernel code, 1240K rwdata, 5496K rodata, 2624K init, 1014K bss, 45428K reserved, 327680K cma-)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4.
[ 0.000000] Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: 512 SPIs implemented
[ 0.000000] GICv3: 0 Extended SPIs implemented
[ 0.000000] GICv3: Distributor has no Range Selector support
[ 0.000000] GICv3: 16 PPIs implemented
[ 0.000000] GICv3: no VLPI support, no direct LPI support
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000051b00000
[ 0.000000] random: get_random_bytes called from start_kernel+0x2b8/0x44c with crng_init=0
[ 0.000000] arch_timer: cp15 timer(s) running at 8.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1d854df40, max_idle_ns: 440795202120 ns
[ 0.000005] sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 2199023255500ns
[ 0.008912] Console: colour dummy device 80x25
[ 0.013096] Calibrating delay loop (skipped), value calculated using timer frequency.. 16.00 BogoMIPS (lpj=32000)
[ 0.023272] pid_max: default: 32768 minimum: 301
[ 0.027963] LSM: Security Framework initializing
[ 0.032539] Mount-cache hash table entries: 2048 (order: 2, 16384 bytes, linear)
[ 0.039870] Mountpoint-cache hash table entries: 2048 (order: 2, 16384 bytes, linear)
[ 0.071782] ASID allocator initialised with 32768 entries
[ 0.084875] rcu: Hierarchical SRCU implementation.
[ 0.099667] EFI services will not be available.
[ 0.111907] smp: Bringing up secondary CPUs ...
[ 0.148526] Detected VIPT I-cache on CPU1
[ 0.148558] GICv3: CPU1: found redistributor 1 region 0:0x0000000051b20000
[ 0.148597] CPU1: Booted secondary processor 0x0000000001 [0x410fd042]
[ 0.180565] Detected VIPT I-cache on CPU2
[ 0.180587] GICv3: CPU2: found redistributor 2 region 0:0x0000000051b40000
[ 0.180611] CPU2: Booted secondary processor 0x0000000002 [0x410fd042]
[ 0.212625] Detected VIPT I-cache on CPU3
[ 0.212644] GICv3: CPU3: found redistributor 3 region 0:0x0000000051b60000
[ 0.212665] CPU3: Booted secondary processor 0x0000000003 [0x410fd042]
[ 0.212731] smp: Brought up 1 node, 4 CPUs
[ 0.268621] SMP: Total of 4 processors activated.
[ 0.273309] CPU features: detected: 32-bit EL0 Support
[ 0.278451] CPU features: detected: CRC32 instructions
[ 0.289659] CPU: All CPU(s) started at EL2
[ 0.293443] alternatives: patching kernel code
[ 0.299023] devtmpfs: initialized
[ 0.318862] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.328289] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
[ 0.345221] pinctrl core: initialized pinctrl subsystem
[ 0.350951] DMI not present or invalid.
[ 0.354775] NET: Registered protocol family 16
[ 0.372544] DMA: preallocated 256 KiB pool for atomic allocations
[ 0.378339] audit: initializing netlink subsys (disabled)
[ 0.383951] audit: type=2000 audit(0.328:1): state=initialized audit_enabled=0 res=1
[ 0.391454] cpuidle: using governor menu
[ 0.396276] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.404729] Serial: AMBA PL011 UART driver
[ 0.408562] imx mu driver is registered.
[ 0.412405] imx rpmsg driver is registered.
[ 0.473041] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
[ 0.479437] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
[ 0.486097] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.492786] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
[ 0.501518] cryptd: max_cpu_qlen set to 1000
[ 0.512544] ACPI: Interpreter disabled.
[ 0.518525] iommu: Default domain type: Translated
[ 0.523444] SCSI subsystem initialized
[ 0.527569] usbcore: registered new interface driver usbfs
[ 0.532762] usbcore: registered new interface driver hub
[ 0.538068] usbcore: registered new device driver usb
[ 0.545565] mc: Linux media interface: v0.10
[ 0.549555] videodev: Linux video capture interface: v2.00
[ 0.555023] pps_core: LinuxPPS API ver. 1 registered
[ 0.559923] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.569060] PTP clock support registered
[ 0.573362] EDAC MC: Ver: 3.0.0
[ 0.577933] No BMan portals available!
[ 0.581738] QMan: Allocated lookup table at (____ptrval____), entry count 65537
[ 0.589444] No QMan portals available!
[ 0.593932] No USDPAA memory, no 'fsl,usdpaa-mem' in device-tree
[ 0.601076] FPGA manager framework
[ 0.604258] Advanced Linux Sound Architecture Driver Initialized.
[ 0.612031] imx-scu scu: NXP i.MX SCU Initialized
[ 0.622154] random: fast init done
[ 0.658017] imx8qxp-pinctrl scu:pinctrl: Invalid fsl,pins or pins property in node /scu/pinctrl/cm40i2cgrp-gpio
[ 0.667788] imx8qxp-pinctrl scu:pinctrl: Invalid fsl,pins or pins property in node /scu/pinctrl/mipi_lvds1_i2c0_grp
[ 0.678306] imx8qxp-pinctrl scu:pinctrl: Invalid fsl,pins or pins property in node /scu/pinctrl/wifi_initgrp
[ 0.688025] imx8qxp-pinctrl scu:pinctrl: initialized IMX pinctrl driver
[ 0.696805] clocksource: Switched to clocksource arch_sys_counter
[ 0.702794] VFS: Disk quotas dquot_6.6.0
[ 0.706534] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 0.714646] pnp: PnP ACPI: disabled
[ 0.748942] thermal_sys: Registered thermal governor 'step_wise'
[ 0.748947] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.755180] NET: Registered protocol family 2
[ 0.766105] tcp_listen_portaddr_hash hash table entries: 512 (order: 1, 8192 bytes, linear)
[ 0.774163] TCP established hash table entries: 8192 (order: 4, 65536 bytes, linear)
[ 0.781923] TCP bind hash table entries: 8192 (order: 5, 131072 bytes, linear)
[ 0.789184] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.795498] UDP hash table entries: 512 (order: 2, 16384 bytes, linear)
[ 0.802036] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes, linear)
[ 0.809191] NET: Registered protocol family 1
[ 0.813835] RPC: Registered named UNIX socket transport module.
[ 0.819436] RPC: Registered udp transport module.
[ 0.824120] RPC: Registered tcp transport module.
[ 0.828803] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.836471] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
[ 0.845172] kvm [1]: IPA Size Limit: 40bits
[ 0.849686] kvm [1]: GICv3: no GICV resource entry
[ 0.854140] kvm [1]: disabling GICv2 emulation
[ 0.858580] kvm [1]: GIC system register CPU interface enabled
[ 0.864469] kvm [1]: vgic interrupt IRQ1
[ 0.868420] kvm [1]: Hyp mode initialized successfully
[ 0.880259] Initialise system trusted keyrings
[ 0.884525] workingset: timestamp_bits=44 max_order=18 bucket_order=0
[ 0.898248] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.904557] NFS: Registering the id_resolver key type
[ 0.909308] Key type id_resolver registered
[ 0.913491] Key type id_legacy registered
[ 0.917456] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 0.924161] jffs2: version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.
[ 0.930686] 9p: Installing v9fs 9p2000 file system support
[ 0.953073] Key type asymmetric registered
[ 0.956837] Asymmetric key parser 'x509' registered
[ 0.961729] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245)
[ 0.969080] io scheduler mq-deadline registered
[ 0.973597] io scheduler kyber registered
[ 0.992395] imx8qxp-pinctrl scu:pinctrl: pin IMX8QXP_MIPI_DSI1_GPIO0_00 already requested by scu:pinctrl; cannot claim for 56244000.pwm
[ 1.004256] imx8qxp-pinctrl scu:pinctrl: pin-122 (56244000.pwm) status -22
[ 1.011108] imx8qxp-pinctrl scu:pinctrl: could not request pin 122 (IMX8QXP_MIPI_DSI1_GPIO0_00) from group mipi_lvds1_pwm_grp on device scu:pinctrl
[ 1.024397] pwm-imx27 56244000.pwm: Error applying setting, reverse things back
[ 1.031700] pwm-imx27: probe of 56244000.pwm failed with error -22
[ 1.039475] EINJ: ACPI disabled.
[ 1.122862] mxs-dma 5b810000.dma-apbh: initialized
[ 1.131266] Bus freq driver module loaded
[ 1.140943] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 1.152616] 5a060000.serial: ttyLP0 at MMIO 0x5a060010 (irq = 58, base_baud = 5000000) is a FSL_LPUAR[ 1.161794] printk: console [ttyLP0] enabled
[ 1.161794] printk: console [ttyLP0] enabled
[ 1.170205] printk: bootconsole [lpuart32] disabled
[ 1.170205] printk: bootconsole [lpuart32] disabled
[ 1.180307] fsl-lpuart 5a060000.serial: DMA tx channel request failed, operating without tx DMA
[ 1.189068] fsl-lpuart 5a060000.serial: DMA rx channel request failed, operating without rx DMA
[ 1.198367] 5a070000.serial: ttyLP1 at MMIO 0x5a070010 (irq = 59, base_baud = 5000000) is a FSL_LPUART
[ 1.208737] 5a080000.serial: ttyLP2 at MMIO 0x5a080010 (irq = 60, base_baud = 5000000) is a FSL_LPUART
[ 1.219074] 5a090000.serial: ttyLP3 at MMIO 0x5a090010 (irq = 61, base_baud = 5000000) is a FSL_LPUART
[ 1.291683] loop: module loaded
[ 1.299087] imx ahci driver is registered.
[ 1.312358] imx8qxp-pinctrl scu:pinctrl: pin IMX8QXP_QSPI0B_SCLK already requested by scu:pinctrl; cannot claim for 5d120000.spi
[ 1.323969] imx8qxp-pinctrl scu:pinctrl: pin-165 (5d120000.spi) status -22
[ 1.330869] imx8qxp-pinctrl scu:pinctrl: could not request pin 165 (IMX8QXP_QSPI0B_SCLK) from group flexspi0grp on device scu:pinctrl
[ 1.342975] nxp-fspi 5d120000.spi: Error applying setting, reverse things back
[ 1.350233] nxp-fspi: probe of 5d120000.spi failed with error -22
[ 1.358910] libphy: Fixed MDIO Bus: probed
[ 1.364046] tun: Universal TUN/TAP device driver, 1.6
[ 1.373868] pps pps0: new PPS source ptp0
[ 1.386171] Freescale FM module, FMD API version 21.1.0
[ 1.392406] Freescale FM Ports module
[ 1.396080] fsl_mac: fsl_mac: FSL FMan MAC API based driver
[ 1.402234] fsl_dpa: FSL DPAA Ethernet driver
[ 1.406997] fsl_advanced: FSL DPAA Advanced drivers:
[ 1.411975] fsl_proxy: FSL DPAA Proxy initialization driver
[ 1.417946] fsl_oh: FSL FMan Offline Parsing port driver
[ 1.428413] VFIO - User Level meta-driver version: 0.3
[ 1.442470] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 1.449036] ehci-platform: EHCI generic platform driver
[ 1.454982] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
[ 1.461203] ohci-platform: OHCI generic platform driver
[ 1.468565] usbcore: registered new interface driver usb-storage
[ 1.474694] usbcore: registered new interface driver usbserial_generic
[ 1.481251] usbserial: USB Serial support registered for generic
[ 1.487299] usbcore: registered new interface driver ftdi_sio
[ 1.493080] usbserial: USB Serial support registered for FTDI USB Serial Device
[ 1.500431] usbcore: registered new interface driver usb_serial_simple
[ 1.507078] usbserial: USB Serial support registered for carelink
[ 1.513209] usbserial: USB Serial support registered for zio
[ 1.518900] usbserial: USB Serial support registered for funsoft
[ 1.524940] usbserial: USB Serial support registered for flashloader
[ 1.531323] usbserial: USB Serial support registered for google
[ 1.537273] usbserial: USB Serial support registered for libtransistor
[ 1.543835] usbserial: USB Serial support registered for vivopay
[ 1.549872] usbserial: USB Serial support registered for moto_modem
[ 1.556174] usbserial: USB Serial support registered for motorola_tetra
[ 1.562813] usbserial: USB Serial support registered for novatel_gps
[ 1.569199] usbserial: USB Serial support registered for hp4x
[ 1.574978] usbserial: USB Serial support registered for suunto
[ 1.580930] usbserial: USB Serial support registered for siemens_mpi
[ 1.596205] input: sc-powerkey as /devices/platform/sc-powerkey/input/input0
[ 1.607214] imx-sc-rtc scu:rtc: registered as rtc0
[ 1.613619] i2c /dev entries driver
[ 1.635514] sdhci: Secure Digital Host Controller Interface driver
[ 1.641737] sdhci: Copyright(c) Pierre Ossman
[ 1.646569] Synopsys Designware Multimedia Card Interface Driver
[ 1.654779] sdhci-pltfm: SDHCI platform and OF driver helper
[ 1.662777] mmc0: CQHCI version 5.10
[ 1.699268] mmc0: SDHCI controller on 5b010000.mmc [5b010000.mmc] using ADMA
[ 1.707625] mmc1: CQHCI version 5.10
[ 1.716809] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.725827] caam 31400000.crypto: device ID = 0x0a16040000000100 (Era 9)
[ 1.732605] caam 31400000.crypto: job rings = 2, qi = 0
[ 1.758716] caam algorithms registered in /proc/crypto
[ 1.766995] caam 31400000.crypto: caam pkc algorithms registered in /proc/crypto
[ 1.775380] caam_jr 31430000.jr: registering rng-caam
[ 1.785693] usbcore: registered new interface driver usbhid
[ 1.791544] usbhid: USB HID core driver
[ 1.798713] No fsl,qman node
[ 1.801629] Freescale USDPAA process driver
[ 1.805821] fsl-usdpaa: no region found
[ 1.809668] Freescale USDPAA process IRQ driver
[ 1.827607] Galcore version 6.4.0.234062
[ 1.830208] mmc0: new HS400 MMC card at address 0001
[ 1.837583] mmcblk0: mmc0:0001 IS032G 29.1 GiB
[ 1.842512] mmcblk0boot0: mmc0:0001 IS032G partition 1 4.00 MiB
[ 1.848690] mmcblk0boot1: mmc0:0001 IS032G partition 2 4.00 MiB
[ 1.854837] mmcblk0rpmb: mmc0:0001 IS032G partition 3 4.00 MiB, chardev (239:0)
[ 1.873436] mmcblk0: p1 p2
[ 1.988482] pktgen: Packet Generator for packet performance testing. Version: 2.75
[ 1.996588] NET: Registered protocol family 26
[ 2.001793] NET: Registered protocol family 10
[ 2.007083] Segment Routing with IPv6
[ 2.010827] NET: Registered protocol family 17
[ 2.015325] 8021q: 802.1Q VLAN Support v1.8
[ 2.019659] 9pnet: Installing 9P2000 support
[ 2.023999] tsn generic netlink module v1 init...
[ 2.028809] Key type dns_resolver registered
[ 2.033548] registered taskstats version 1
[ 2.037681] Loading compiled-in X.509 certificates
[ 2.081464] gpio-42 (scl): enforced open drain please flag it properly in DT/ACPI DSDT/board file
[ 2.090391] imx-lpi2c 37230000.i2c: using scl,sda for recovery
[ 2.099363] i2c i2c-16: LPI2C adapter registered
[ 2.105748] i2c i2c-17: LPI2C adapter registered
[ 2.112072] i2c i2c-18: LPI2C adapter registered
[ 2.117449] imx-lpi2c 56226000.i2c: can't get irq number
[ 2.124317] imx-lpi2c 56246000.i2c: can't get irq number
[ 2.138945] dpu-core 56180000.dpu: driver probed
[ 2.145384] pps pps0: new PPS source ptp0
[ 2.155468] fec 5b040000.ethernet: Invalid MAC address: 00:00:00:00:00:00
[ 2.162348] fec 5b040000.ethernet: Using random MAC address: e6:5c:99:7c:6b:c4
[ 2.170505] libphy: fec_enet_mii_bus: probed
[ 2.174938] mdio_bus 5b040000.ethernet-1: MDIO device at address 0 is missing.
[ 2.183012] fec 5b040000.ethernet eth0: registered PHC device 0
[ 2.255857] mmc1: CQHCI version 5.10
[ 2.259545] sdhci-esdhc-imx 5b020000.mmc: Got CD GPIO
[ 2.264645] sdhci-esdhc-imx 5b020000.mmc: Got WP GPIO
[ 2.301702] mmc1: SDHCI controller on 5b020000.mmc [5b020000.mmc] using ADMA
[ 2.340028] it6263 19-004c: Probe failed. Remote port 'lvds-channel@0' disabled
[ 2.347577] i2c i2c-19: LPI2C adapter registered
[ 3.383674] it6263 20-004c: Probe failed. Remote port 'lvds-channel@0' disabled
[ 3.391223] i2c i2c-20: LPI2C adapter registered
[ 3.404027] debugfs: Directory 'lvds1' with parent 'pm_genpd' already present!
[ 3.411371] debugfs: Directory 'mipi1-i2c1' with parent 'pm_genpd' already present!
[ 3.419055] debugfs: Directory 'mipi1-i2c0' with parent 'pm_genpd' already present!
[ 3.426749] debugfs: Directory 'mipi1-pwm0' with parent 'pm_genpd' already present!
[ 3.434423] debugfs: Directory 'mipi1' with parent 'pm_genpd' already present!
[ 3.449712] imx-sc-rtc scu:rtc: setting system clock to 1970-01-01T00:00:10 UTC (10)
[ 3.457911] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[ 3.466860] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[ 3.473509] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
[ 3.482163] platform regulatory.0: Falling back to sysfs fallback for: regulatory.db
[ 3.497189] ALSA device list:
[ 3.500165] No soundcards found.
[ 3.558378] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 3.566906] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 3.573522] devtmpfs: mounted
[ 3.577526] Freeing unused kernel memory: 2624K
[ 3.582127] Run /sbin/init as init process
[ 3.676975] systemd[1]: System time before build time, advancing clock.
[ 3.696237] systemd[1]: systemd 243.2+ running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -)
[ 3.718503] systemd[1]: Detected architecture arm64.

Welcome to NXP i.MX Release Distro 5.4-zeus (zeus)!

[ 3.769338] systemd[1]: Set hostname to <imx8qxpmek>.
[ 3.778634] random: systemd: uninitialized urandom read (16 bytes read)
[ 3.785674] systemd[1]: Initializing machine ID from random generator.
[ 4.002371] systemd[1]: /lib/systemd/system/dbus.socket:5: ListenStream= references a path below legacy directory /var/run/, updating /var/run/dbus.
[ 4.135583] systemd[1]: /lib/systemd/system/rpcbind.socket:5: ListenStream= references a path below legacy directory /var/run/, updating /var/run/r.
[ 4.166002] random: systemd: uninitialized urandom read (16 bytes read)
[ 4.172853] systemd[1]: system-getty.slice: unit configures an IP firewall, but the local system does not support BPF/cgroup firewalling.
[ 4.185269] systemd[1]: (This warning is only shown for the first unit using IP firewalling.)
[ 4.196676] systemd[1]: Created slice system-getty.slice.
[ OK ] Created slice system-getty.slice.
[ 4.213037] random: systemd: uninitialized urandom read (16 bytes read)
[ 4.221177] systemd[1]: Created slice system-serial\x2dgetty.slice.
[ OK ] Created slice system-serial\x2dgetty.slice.
[ OK ] Created slice User and Session Slice.
[ OK ] Started Dispatch Password ��…ts to Console Directory Watch.
[ OK ] Started Forward Password R��…uests to Wall Directory Watch.
[ OK ] Reached target Paths.
[ OK ] Reached target Remote File Systems.
[ OK ] Reached target Slices.
[ OK ] Reached target Swap.
[ OK ] Listening on Syslog Socket.
[ OK ] Listening on initctl Compatibility Named Pipe.
[ OK ] Listening on Journal Audit Socket.
[ OK ] Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket.
[ OK ] Listening on Network Service Netlink Socket.
[ OK ] Listening on udev Control Socket.
[ OK ] Listening on udev Kernel Socket.
Mounting Huge Pages File System...
Mounting POSIX Message Queue File System...
Mounting Kernel Debug File System...
Mounting Temporary Directory (/tmp)...
Starting Create list of st��…odes for the current kernel...
Starting Journal Service...
Mounting Kernel Configuration File System...
Starting Remount Root and Kernel File Systems...
[ 4.575764] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
Starting Apply Kernel Variables...
[ 4.586895] ext4 filesystem being remounted at / supports timestamps until 2038 (0x7fffffff)
Starting udev Coldplug all Devices...
Starting Setup Virtual Console...
[ OK ] Started Journal Service.
[ OK ] Mounted Huge Pages File System.
[ OK ] Mounted POSIX Message Queue File System.
[ OK ] Mounted Kernel Debug File System.
[ OK ] Mounted Temporary Directory (/tmp).
[ OK ] Started Create list of sta��… nodes for the current kernel.
[ OK ] Mounted Kernel Configuration File System.
[ OK ] Started Remount Root and Kernel File Systems.
[ OK ] Started Apply Kernel Variables.
[ OK ] Started Setup Virtual Console.
Starting Flush Journal to Persistent Storage...
[ 4.819336] systemd-journald[427]: Received client request to flush runtime journal.
Starting Create System Users...
[ OK ] Started Flush Journal to Persistent Storage.
[ OK ] Started Create System Users.
Starting Create Static Device Nodes in /dev...
[ OK ] Started Create Static Device Nodes in /dev.
[ OK ] Reached target Local File Systems (Pre).
Mounting /var/volatile...
Starting udev Kernel Device Manager...
[ OK ] Mounted /var/volatile.
Starting Load/Save Random Seed...
[ OK ] Reached target Local File Systems.
Starting Rebuild Dynamic Linker Cache...
Starting Create Volatile Files and Directories...
[ OK ] Started udev Kernel Device Manager.
Starting Network Service...
[ OK ] Started Create Volatile Files and Directories.
Starting Run pending postinsts...
Starting Rebuild Journal Catalog...
Starting Network Time Synchronization...
Starting Update UTMP about System Boot/Shutdown...
[ OK ] Started Network Service.
[ OK ] Started Update UTMP about System Boot/Shutdown.
Starting Network Name Resolution...
[ OK ] Started Rebuild Journal Catalog.
[ OK ] Started Rebuild Dynamic Linker Cache.
Starting Update is Completed...
[ OK ] Started udev Coldplug all Devices.
[ OK ] Started Update is Completed.
Starting Start Psplash Boot Screen...
[ OK ] Started Start Psplash Boot Screen.
[ OK ] Started Network Time Synchronization.
[ OK ] Reached target System Time Set.
[ OK ] Reached target System Time Synchronized.
[ OK ] Started Network Name Resolution.
[ OK ] Started Run pending postinsts.
[ OK ] Reached target Network.
[ OK ] Reached target Host and Network Name Lookups.
[ OK ] Reached target System Initialization.
[ OK ] Started Daily apt download activities.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Reached target Timers.
[ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[ OK ] Listening on D-Bus System Message Bus Socket.
[ OK ] Listening on RPCbind Server Activation Socket.
[ OK ] Reached target Sockets.
[ OK ] Reached target Basic System.
[ 5.649989] [VPU Encoder] enable mu for core[0]
[ 5.663057] [VPU Encoder] vpu encoder core[0] firmware version is 1.2.7
Starting Avahi mDNS/DNS-SD Stack...
[ OK ] Started Kernel Logging Service.
[ OK ] Started System Logging Service.
[ OK ] Started D-Bus System Message Bus.
Starting Telephony service...
[ OK ] Started Updates psplash to basic.
[ OK ] Started Update psplash to network.
Starting Terminate Psplash Boot Screen...
[ OK ] Started User Space Regulatory Firmware Loading.
[ OK ] Started User Space SDMA Firmware Loading.
Starting Login Service...
Starting Permit User Sessions...
[ OK ] Started TEE Supplicant.
[FAILED] Failed to start Terminate Psplash Boot Screen.
See 'systemctl status psplash-quit.service' for details.
[ OK ] Started Permit User Sessions.
[ 6.050536] fec 5b040000.ethernet eth0: Unable to connect to phy
[ OK ] Started Avahi mDNS/DNS-SD Stack.
[ OK ] Started Telephony service.
[ OK ] Started Login Service.
[ OK ] Created slice system-systemd\x2dbacklight.slice.
[ OK ] Started Getty on tty1.
[ OK ] Started Serial Getty on ttyLP0.
[ OK ] Reached target Login Prompts.
[ OK ] Reached target Multi-User System.
Starting Load/Save Screen ��… backlight:lvds_backlight@0...
Starting Update UTMP about System Runlevel Changes...
[ OK ] Started Load/Save Screen B��…of backlight:lvds_backlight@0.
[ OK ] Started Update UTMP about System Runlevel Changes.
[ 9.832842] random: crng init done
[ 9.836258] random: 7 urandom warning(s) missed due to ratelimiting
[ OK ] Started Load/Save Random Seed.

NXP i.MX Release Distro 5.4-zeus imx8qxpmek ttyLP0

imx8qxpmek login:

0 Kudos
Reply

3,142 Views
igorpadykov
NXP Employee
NXP Employee

for for error "error "it6263 19-004c: Probe failed" - do you have it6263 on custom

board. If not one can remove its codes.

 

Best regards
igor

0 Kudos
Reply