iMX8QXP External clock sources疑问

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8QXP External clock sources疑问

503 Views
jiazhichao
Contributor I

你好

我在IMX8QXPAEC.pdf手册 4.1.4 External clock sources中看到,RTC_XTALI可以使用晶体或外部时钟,但XTALI只描述了可以使用外部24M晶体。
是否24M时钟只能使用外部晶体的方式提供?如果可以使用外部晶振的方式提供,是否从XTALI输入,XTALO悬空?

谢谢!

0 Kudos
Reply
2 Replies

483 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

Yes, for i.MX8QXP you must use an external 24MHZ crystal/clock for correct operation. You can check the corresponding connection in MEK board design files.

Best regards.

0 Kudos
Reply

52 Views
jiazhichao
Contributor I
你好
24MHz我能使用外部有源晶振吗,如果使用外部晶振提供24MHz时钟,我该如何连接呢?XTALI输入,XTALO悬空还是电阻下拉到地呢?
我看到手册里面24MHz时钟这块的地和系统地不同,那么外部晶振的地该怎么接呢,接到VSS_SCU_XTAL吗?
0 Kudos
Reply