iMX8QM part number printed on chip, can't exact match it ..

cancel
Showing results for 
Search instead for 
Did you mean: 

iMX8QM part number printed on chip, can't exact match it ..

278 Views
dry
Senior Contributor I

This is what is printed on my SoC:

dry_0-1663645963505.png

 

This is NXP' product selector:

https://www.nxp.com/products/product-selector:PRODUCT-SELECTOR#/category/c731_c380_c127_c1430

Can't see what that "7" at the end is... Does it matter ? What is the number 7,  datasheet has no number option at the end:

dry_1-1663646092227.png

 

 

0 Kudos
3 Replies

266 Views
b45499
NXP TechSupport
NXP TechSupport

Dear @dry You do not need to care about it, as the product you mention is not our production product, it is for sample. So that you can not see the details in our datasheet.

 

Wish you have a nice day

Best Regards

Rita

0 Kudos

264 Views
dry
Senior Contributor I

Hello @b45499 

Thank you for the info, question:

do we need to worry about using the sample and not production version ...?

0 Kudos

261 Views
b45499
NXP TechSupport
NXP TechSupport

I think you can use it, but for product use recommend you to use the production product in our website.

https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-proces...

Hope this can do help for you

0 Kudos