While building sdk , with bitbake -c populate_sdk fails, with error (at least one ..) being related to dnf ...:
ERROR: Could not invoke dnf. Command '/devel2/linux/imx8/kontron/kci1-smx8-bsp-4.19.35-dev-27c53b5be168/build/tmp/work/kontron_samx8_qm-poky-linux/kontron-image-validation-samx/1.0-r0/recipe-sysroot-native/usr/bin/dnf -v
And checking that file its trying to use :
/devel2/linux/imx8/kontron/kci1-smx8-bsp-4.19.35-dev-27c53b5be168/build/tmp/work/kontron_samx8_qm-poky-linux/kontron-image-validation-samx/1.0-r0/recipe-sysroot-native/usr/bin/dnf
Traceback (most recent call last):
File "/devel2/linux/imx8/kontron/kci1-smx8-bsp-4.19.35-dev-27c53b5be168/build/tmp/work/kontron_samx8_qm-poky-linux/kontron-image-validation-samx/1.0-r0/recipe-sysroot-native/usr/bin/dnf.real", line 57, in <module>
from dnf.cli import main
ModuleNotFoundError: No module named 'dnf'
Additionally, at the end it goes these errors:
Transaction Summary
================================================================================
Install 1490 Packages
Total size: 938 M
Installed size: 5.7 G
Downloading Packages:
Running transaction check
Transaction check succeeded.
Running transaction test
Error: Transaction check error:
file /lib/firmware/qca/NOTICE.txt from install of linux-firmware-qca-1:0.0+git0+711d3297ba_a0026b646c+f6d0859f94-r0.noarch conflicts with file from package firmware-samx8-qca-1.0-r0.noarch
file /lib/firmware/qca/nvm_usb_00000302.bin from install of linux-firmware-qca-1:0.0+git0+711d3297ba_a0026b646c+f6d0859f94-r0.noarch conflicts with file from package firmware-samx8-qca-1.0-r0.noarch
file /lib/firmware/qca/rampatch_usb_00000302.bin from install of linux-firmware-qca-1:0.0+git0+711d3297ba_a0026b646c+f6d0859f94-r0.noarch conflicts with file from package firmware-samx8-qca-1.0-r0.noarch
Error Summary
-------------
So that is broken, and by the looks its file part of Yocto sources.
I'm using NXP's imx docker container, with Ubuntu 18 in it. The actual Yocto distro builds, but not the wanted SDK.
Anyone seen it / knows about how to solve this? Log file is attached.
NXP support ..?