Hi guys, there is a pull-down resistor required on both USB_OTG2_REXT and USB_SS3_REXT.
Technical Datasheet (Rev 0, 10/2019) page 83 specifies 500R 0.5% (497.5Ω to 502.5Ω).
Hardware Developers Guide (v0.6, 01/2019) page 20 specifies 499R 1% (494Ω to 504Ω)
I don't think this is going to be an issue, but thought I would ask anyway to clarify which is correct and to let you know that the documentation should be changed to agree with each other.
Regards,
Peter
Hello,
Use the recent Datasheet(s) with hardware specs.
i.MX 8 Family Applications Processor | Arm Cortex-A53/A72/M4 | NXP
Note, the HDG is not published yet.
Have a great day,
Yuri
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.