iMX8QM Multiple displays

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8QM Multiple displays

560件の閲覧回数
pierluigi_p
Contributor V

Dear NXP team,

from the imx8qm-mek.dts sample device tree, I can guess that 2 distinct displays can be driven simultaneously when linked to 2 different DPUs.

If I understand correctly the imx8qm-ss-dc.dtsi device tree, each DPU provides 2 ports and each port (but port0 of dpu2) provides 2 endpoints: totally I can see 7 endpoints.

Can all the 7 endpoints be used simultaneously?

More generally, for a specific port, can I use both the endpoints?

If not, can I simultaneously use 1 endpoint for each port (4 endpoints)?

Is there any reference documentation about the possible use of DPUs/ports/endpoints?

Thanks

Best Regards

Pier

ラベル(1)
2 返答(返信)

550件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @pierluigi_p 

 

Display Controller Supports single UltraHD 4Kp60 display or up to 4 independent FullHD 1080p60
displays

Display I/O

2× MIPI-DSI with 4 lanes each
1× HDMI-TX/DisplayPort compliant with:
• HDMI
• eDP 1.4
• DP 1.3
This high performance serializer supports a pair of LVDS displays with 8 lanes each.
Each port can be configured for 2x Tx with 4 lanes each.

dpu1 and dpu2 are two different definitions. You can't use dpu2 when using dpu1.

So the max number of screen is 4 if you want to display 4 different contents.

The lvds0 ch0 and ch1 share same rgb data, you can use connect 2 display devices to lvds0. But they display same content.

 

Is there any reference documentation about the possible use of DPUs/ports/endpoints?

--->See i.mx8qm datasheet

0 件の賞賛

541件の閲覧回数
pierluigi_p
Contributor V

Hi @Zhiming_Liu,

according the iMX8QM datasheet, I understand I can get 4 displays, one for each port, 2 from dpu1 and 2 from dpu2, is this correct?

How can I get 4 displays if I "can't use dpu2 when using dpu1" ?

Thanks

Best Regards

Pier