Hello Community!
I am developing an ISP board that connects to iMX8QM MEK.
The hardware configuration diagram is below.
The software is Linux 6.1.22, and the sensor driver is created based on gmsl-max9286.c.
Now I get an exception when starting Linux.
The sensor board outputs virtual channel 2ch via MIPI, and I have an inquiry regarding the kernel 2ch settings.
[ question 1 ]
I changed the kernel dts and sensor driver as shown below, but are there any mistakes in the settings?
dts:
&isi_0 {
status = "okay";
cap_device {
status = "okay";
};
m2m_device {
status = "okay";
};
};
&isi_1 {
status = "okay";
cap_device {
status = "okay";
};
};
&isi_2 {
status = "disabled"; //[sdi] to disabled
cap_device {
status = "disabled"; //[sdi] to disabled
};
};
&isi_3 {
status = "disabled"; //[sdi] to disabled
cap_device {
status = "disabled"; //[sdi] to disabled
};
};
&isi_4 {
status = "disabled"; //[sdi] to disabled
cap_device {
status = "disabled"; //[sdi] to disabled
};
};
&isi_5 {
status = "disabled"; //[sdi] to disabled
cap_device {
status = "disabled"; //[sdi] to disabled
};
};
&isi_6 {
status = "disabled"; //[sdi] to disabled
cap_device {
status = "disabled"; //[sdi] to disabled
};
};
&isi_7 {
status = "disabled"; //[sdi] to disabled
cap_device {
status = "disabled"; //[sdi] to disabled
};
};
&mipi_csi_0 {
#address-cells = <1>;
#size-cells = <0>;
virtual-channel;
status = "okay";
/* Camera 0 MIPI CSI-2 (CSIS0) */
port@0 {
reg = <0>;
mipi_csi0_ep: endpoint {
remote-endpoint = <&max9286_0_ep>;
data-lanes = <1 2 3 4>;
};
};
};
&i2c_mipi_csi0 {
#address-cells = <1>;
#size-cells = <0>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_i2c_mipi_csi0>;
clock-frequency = <100000>;
status = "okay";
max9286_mipi@6a {
compatible = "sdi,isp_mipi";
reg = <0x6a>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_mipi_csi0>;
clocks = <&clk_dummy>;
clock-names = "capture_mclk";
mclk = <27000000>;
mclk_source = <0>;
pwn-gpios = <&lsio_gpio1 27 GPIO_ACTIVE_HIGH>;
virtual-channel;
status = "okay";
port {
max9286_0_ep: endpoint {
remote-endpoint = <&mipi_csi0_ep>;
data-lanes = <1 2 3 4>;
};
};
};
};
senser driver probe function:
#define MIPI_CSI2_SENS_VC0_PAD_SOURCE 0
#define MIPI_CSI2_SENS_VC1_PAD_SOURCE 1
#define MIPI_CSI2_SENS_VC2_PAD_SOURCE 2
#define MIPI_CSI2_SENS_VCX_PADS_NUM 2
struct sensor_data {
:
struct media_pad pads[MIPI_CSI2_SENS_VCX_PADS_NUM];
:
}
sd->flags |= V4L2_SUBDEV_FL_HAS_DEVNODE;
sd->entity.function = MEDIA_ENT_F_CAM_SENSOR;
max9286_data->pads[MIPI_CSI2_SENS_VC0_PAD_SOURCE].flags = MEDIA_PAD_FL_SOURCE;
max9286_data->pads[MIPI_CSI2_SENS_VC1_PAD_SOURCE].flags = MEDIA_PAD_FL_SOURCE;
retval = media_entity_pads_init(&sd->entity, MIPI_CSI2_SENS_VCX_PADS_NUM, max9286_data->pads);
Linux dmesg:
[ 2.428771] isp_mipi 2-006a: isp_mipi is found, name isp_mipi 2-006a
[ 10.169351] imx8_media_dev: module is from the staging directory, the quality is unknown, you have been warned.
[ 10.196793] mx8-img-md: Registered mxc_isi.0.capture as /dev/video3
[ 10.214497] mx8-img-md: Registered mxc_isi.1.capture as /dev/video4
[ 10.221031] mx8-img-md: Registered sensor subdevice: isp_mipi_cam 2-006a (1)
[ 10.241443] mx8-img-md: created link [mxc_isi.0] => [mxc_isi.0.capture]
[ 10.285198] mx8-img-md: created link [mxc-mipi-csi2.0] => [mxc_isi.0]
[ 10.304164] mx8-img-md: created link [mxc_isi.1] => [mxc_isi.1.capture]
[ 10.323244] mx8-img-md: created link [mxc-mipi-csi2.0] => [mxc_isi.1]
[ 10.364732] ------------[ cut here ]------------
[ 10.369366] WARNING: CPU: 0 PID: 337 at drivers/media/mc/mc-entity.c:1021 media_create_pad_link+0x8c/0x220
[ 10.379044] Modules linked in: flexcan(+) can_dev snd_soc_fsl_sai(+) snd_soc_fsl_audmix imx8_media_dev(C+) snd_soc_fsl_asrc snd_soc_fsl_utils snd_soc_fsl_esai caam error imx_dsp_rproc fuse
[ 10.395873] CPU: 0 PID: 337 Comm: (udev-worker) Tainted: G C 6.1.22 #51
[ 10.403888] Hardware name: Freescale i.MX8QM MEK (DT)
[ 10.408945] pstate: 60000005 (nZCv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[ 10.415911] pc : media_create_pad_link+0x8c/0x220
[ 10.420629] lr : media_create_pad_link+0x58/0x220
[ 10.425338] sp : ffff80000c1db6f0
[ 10.428655] x29: ffff80000c1db6f0 x28: ffff000811dcd080 x27: ffff0008119e0880
[ 10.435805] x26: 0000000000000004 x25: 0000000000000040 x24: ffff00081a5d6650
[ 10.442954] x23: 0000000000000002 x22: 0000000000000002 x21: 0000000000000003
[ 10.450096] x20: ffff000811dcd080 x19: ffff0008119e0880 x18: 0000000000000006
[ 10.457245] x17: 730a323d6461705f x16: 6b6e697320323d64 x15: 61705f656372756f
[ 10.464386] x14: 7320383639333836 x13: 383d736461705f6d x12: 756e3e2d6b6e6973
[ 10.471527] x11: 20323d736461705f x10: 0000000000000a70 x9 : ffff8000081e329c
[ 10.478668] x8 : ffff0008155655d0 x7 : 0000000000000000 x6 : 0000000000000015
[ 10.485809] x5 : ffff0008ff32ea18 x4 : ffff0008ff32ea18 x3 : 0000000000000000
[ 10.492950] x2 : 0000000000000000 x1 : ffff000815564b00 x0 : 0000000000000002
[ 10.500092] Call trace:
[ 10.502535] media_create_pad_link+0x8c/0x220
[ 10.506903] subdev_notifier_complete+0x4ac/0x6c0 [imx8_media_dev]
[ 10.513106] v4l2_async_nf_try_complete+0x84/0x9c
[ 10.517823] __v4l2_async_nf_register+0xe8/0x140
[ 10.522444] v4l2_async_nf_register+0x4c/0x74
[ 10.526805] mxc_md_probe+0x674/0xa40 [imx8_media_dev]
[ 10.531957] platform_probe+0x70/0xcc
[ 10.535623] really_probe+0xc8/0x3e0
[ 10.539203] __driver_probe_device+0x84/0x190
[ 10.543564] driver_probe_device+0x44/0x120
[ 10.547751] __driver_attach+0xfc/0x204
[ 10.551591] bus_for_each_dev+0x7c/0xe0
[ 10.555431] driver_attach+0x2c/0x40
[ 10.559010] bus_add_driver+0x184/0x240
[ 10.562850] driver_register+0x80/0x13c
[ 10.566690] __platform_driver_register+0x30/0x3c
[ 10.571399] mxc_md_driver_init+0x28/0x1000 [imx8_media_dev]
[ 10.577071] do_one_initcall+0x60/0x2d0
[ 10.580911] do_init_module+0x50/0x1f0
[ 10.584664] load_module+0x1c44/0x2024
[ 10.588418] __do_sys_finit_module+0xac/0x12c
[ 10.592779] __arm64_sys_finit_module+0x28/0x34
[ 10.597313] invoke_syscall+0x50/0x120
[ 10.601066] el0_svc_common.constprop.0+0xd4/0xf4
[ 10.605775] do_el0_svc+0x34/0xd0
[ 10.609093] el0_svc+0x2c/0x84
[ 10.612154] el0t_64_sync_handler+0xf4/0x120
[ 10.616426] el0t_64_sync+0x18c/0x190
[ 10.620093] ---[ end trace 0000000000000000 ]---
[ 10.636501] mx8-img-md: subdev_notifier_complete error exit
[ 10.642194] mxc-md bus@58000000:camera: Sensor register failed
[ 10.648142] mxc-md: probe of bus@58000000:camera failed with error -22
The causes of the exception are as follows.
drivers/media/mc/mc-entity.c:1035
WARN_ON(source_pad >= source->num_pads) ||This is because source_pad=2, source->num_pads=2.
[ question 2 ]
I think gmsl-max9286.c is virtual channel 4ch. With this 4ch setting, no exception occurs, but is it okay to use the 4ch setting even with 2ch output?
All suggestions welcome.
Best regards.
解決済! 解決策の投稿を見る。
Hi @aso,
I hope you are doing well.
There seem to be redundant nodes of mipi_csi_0 in shared dts.
It looks like virtual channels are hardcoded to 1 or 4 in imx8-media-dev.c driver.
mipi_vc = (mipi_csi2->vchannel) ? 4 : 1;
One can try changing it in /drivers/staging/media/imx/imx8-media-dev.c
Thanks & Regards,
Dhruvit Vasavada
Hi @aso,
I hope you are doing well.
Have you disabled mipi_csi_1 and i2c_mipi_csi1 nodes also?
There seems to be some issue with the configuration of source pad mappings.
Please share the full device tree.
Thanks & Regards,
Dhruvit Vasavada
Hi, @Dhruvit
Thank you for your reply.
Yes, it's disabled.
I have attached a dts file, so please check it.
Best regards.
Hi @aso,
I hope you are doing well.
There seem to be redundant nodes of mipi_csi_0 in shared dts.
It looks like virtual channels are hardcoded to 1 or 4 in imx8-media-dev.c driver.
mipi_vc = (mipi_csi2->vchannel) ? 4 : 1;
One can try changing it in /drivers/staging/media/imx/imx8-media-dev.c
Thanks & Regards,
Dhruvit Vasavada
Hi, @Dhruvit
Thanks for your support.
I modified imx8-media-dev.c and succeeded in avoiding the exception.
Now I started Linux and started debugging the sensor driver, but camera capture fails.
I'll post this issue in a separate thread.
Best regards.