Hello,
I downloaded the Android Automotive OS 12.0.0_2.1.0 prebuilt image for the iMX8QM platform.
I wrote the prebuilt image with the command "sudo ./uuu_imx_android_flash.sh -f imx8qm -u xen -d xen -e -y imx-full-image.wic".
But when the image is standing up, it cannot find the command "run xenmmcboot" in the U-Boot.
I was wondering if Android Automotive OS 12 has XEN support.
Could you please help with this?
Best regards,
Efecan
Hello,
Xen is not building in the prebuilt image, you need build the kernel before use it.
Regards
Hello @Bio_TICFSL,
I built Android Automotive OS 12.0.0_2.1.0.
Then I wrote the image with the same uuu command.
But when I enter "run xenmmcboot" command in U-Boot, I get unknown command error.
Do I need to follow another procedure to include XEN in my image?
Could you please help me with this issue?
Best regards,
Efecan