iMX8QM : LVDS display error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8QM : LVDS display error

1,259 Views
Hyungj
Contributor I

I want to use 2 LVDS display with 2 channel.

So, I fix the imx8qm-XXXX.dts like below and compile it to imx8qm-XXXX.dtb with dtc in Linux

.....

    lvds1_panel { /* LVDS1: LVDS panel */
        compatible = "powertrip,ph128800t004-zhc";
        backlight = <&lvds1_backlight>;
        pinctrl-names = "default";
        pinctrl-0 = <&pinctrl_lvds1>;
        power-supply = <&reg_1p8v>;
        enable-gpios = <&lsio_gpio5 0 GPIO_ACTIVE_HIGH>;
        status = "okay";

        port {
            panel_lvds1_in: endpoint {
                remote-endpoint = <&lvds1_out>;
            };
        };
    };
 
...........
 
&ldb2 { /* LVDS1: LVDS Channel-0 Port Enable */
    status = "okay";
    fsl,dual-channel;

    lvds-channel@0 {
        fsl,data-mapping = "spwg";
        fsl,data-width = <24>;
        status = "okay";
        port@1 {
            reg = <1>;

            lvds1_out: endpoint {
                remote-endpoint = <&panel_lvds1_in>;
            };
        };
    };
};
--------------------
 
Then, I move the file from Host pc to board[run/media/mmcblk0p1] and change the setup in U boot
-setenv fdt_file imx8qm-XXXX.dtb
-saveenv
-boot
 
After booting, I got a looped dmesg error :
[ 11.509961] imx-drm display-subsystem: failed to bind bus@57240000:ldb@572410e0 (ops imx8qm_ldb_ops): -517
[ 11.520191] imx-drm display-subsystem: master bind failed: -517
[ 11.527389] imx-sgtl5000 sound: ASoC: failed to init link HiFi: -517
[ 11.535857] nwl-dsi 56228000.dsi_host: [drm:nwl_dsi_host_attach] lanes=4, format=0x0 flags=0x15
[ 11.544794] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 11.551432] [drm] No driver support for vblank timestamp query.
[ 11.557433] imx-drm display-subsystem: bound imx-drm-dpu-bliteng.2 (ops dpu_bliteng_ops)
[ 11.565592] imx-drm display-subsystem: bound imx-drm-dpu-bliteng.5 (ops dpu_bliteng_ops)
[ 11.573815] imx-drm display-subsystem: bound imx-dpu-crtc.0 (ops dpu_crtc_ops)
[ 11.581155] imx-drm display-subsystem: bound imx-dpu-crtc.1 (ops dpu_crtc_ops)
[ 11.588498] imx-drm display-subsystem: bound imx-dpu-crtc.3 (ops dpu_crtc_ops)
[ 11.595835] imx-drm display-subsystem: bound imx-dpu-crtc.4 (ops dpu_crtc_ops)
[ 11.603480] imx-drm display-subsystem: bound 56228000.dsi_host (ops nwl_dsi_component_ops)
 
 
How can I fix it?
 
0 Kudos
Reply
1 Reply

1,236 Views
joanxie
NXP TechSupport
NXP TechSupport
0 Kudos
Reply