iMX8QM 1200MHz DDR Boot issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8QM 1200MHz DDR Boot issue

2,299 Views
prashanthkumar
Contributor II

Hi,

We are working on iMX8 Quad Max custom board with 4.14.78 Kernel.

Its able to boot from DDR frequency 1600MHz. with following SCFW command.

How to boot  SCFW & u-boot using 1200MHz DDR frequency in kernel?

Can you please provide commands to compile SCFW & Uboot source code.

Regards,

Prashanth Kumar K

0 Kudos
Reply
5 Replies

1,446 Views
prashanthkumar
Contributor II

Hi Igor,

We follow the above mentioned procedure for SCFW compilation.

The compilation command which is we are using as follows.

~# make qm R=B0 B=val M=1 DDR_CON=imx8qmddr4_dcd_1.2GHz

Generating platform/board/mx8qm_val/dcd/imx8qmddr4_dcd_1.2GHz.h
Generating platform/board/mx8qm_val/dcd/dcd.h from platform/board/mx8qm_val/dcd/imx8qmddr4_dcd_1.2GHz.h
Generating platform/board/mx8qm_val/dcd/imx8qmddr4_dcd_1.2GHz_retention.h
Generating platform/board/mx8qm_val/dcd/dcd_retention.h from platform/board/mx8qm_val/dcd/imx8qmddr4_dcd_1.2GHz_retention.h
Compiling platform/drivers/pmic/fsl_pmic.c
Compiling platform/drivers/pmic/pf100/fsl_pf100.c
Compiling platform/drivers/pmic/pf8100/fsl_pf8100.c
Compiling platform/board/mx8qm_val/board.c
Compiling platform/board/board_common.c
Compiling platform/board/pmic.c
Linking build_mx8qm_b0/scfw_tcm.elf ....
Objcopy build_mx8qm_b0/scfw_tcm.bin ....
done.

But while booting iMX8QM board, still its showing as "DDR frequency = 1596000000" instead of "DDR frequency = 1200000000" in SCFW terminal.

The SCFW log is given below for your reference.

DDR frequency = 1596000000
ROM boot time  = 113086 usec
SCFW boot time  = 31611 usec
        Banner  = 13 usec
        Init    = 976 usec
        Config  = 4041 usec
        DDR     = 1319 usec
        SConfig = 231 usec
        Prep    = 22891 usec

Please confirm that SCFW is hard coding the DDR frequency?

Regards,

Prashanth Kumar K

0 Kudos
Reply

1,446 Views
igorpadykov
NXP Employee
NXP Employee

Hi Prashanth 

for DRC( DDR controller/phy) one can find in imx8qmddr4_dcd_1.2GHz.cfg :
    uint32_t rate2 = SC_600MHZ;
    pm_set_clock_rate(SC_PT, SC_R_DRC_0, SC_PM_CLK_MISC0, &rate2);
    pm_set_clock_rate(SC_PT, SC_R_DRC_1, SC_PM_CLK_MISC0, &rate2);

So, were you able to use MX8QM LPDDR4 register programming aid tool

and run ddr test (suggest to obtain it through local nxp office as

this part is not officially released yet).

Best regards
igor

0 Kudos
Reply

1,446 Views
prashanthkumar
Contributor II

Dear Igor,

Attached LPDDR4 stress test log file done with 1200MHz DDR frequency

along with the mail.

Best regards,

Prashanth Kumar K

0 Kudos
Reply

1,446 Views
igorpadykov
NXP Employee
NXP Employee

Hi Prashanth

may be useful to check presentation:

https://community.nxp.com/docs/DOC-341872 

iMX8 Quad Max part is not officially released yet, for custom

design issues suggested to proceed with

NXP Professional Services | NXP 

Best regards
igor

0 Kudos
Reply

1,446 Views
igorpadykov
NXP Employee
NXP Employee

Hi Prashanth

one can check SCFW Porting Kit documentation and 1200MHz example in
scfw_export_mx8qm_b0..mx8dm_val/dcd/imx8dmddr4_dcd_1.2GHz.cfg
SCFW Porting Kit

uboot sources
uboot-imx - i.MX U-Boot 

Note, for custom board cfg file should be generated using MX8QM LPDDR4 register programming

aid and ddr test tool for that part.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply