Hi,
I'm tring to use NFS to mount rootfs at iMX8MQEVK. The images used could boot from emmc normally. When I downloaded the image & dtb by DHCP and mounted the rootfs using NFS, the boot log showed that the board mounted successfully. But it was strange that the rootfs would get stuck as follows:
Dose anyone have idea about this problem?
Thank you !
Hi igorpadykov karan.gajjar@volansystech.com
I tried to mount a simplest rootfs made by myself and it succeeded.
So I think there are too many services that need to be started to cause this stuck.
Thanks & Best Regards
Ida
Hi Ida
one can try steps described in sect.4.7.5 Running the Linux image from NFS
attached Linux Guide with Demo Image
Linux Binary Demo Files - i.MX 8M Quad EVK
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igor ,
Thank you for reply.
I was working on this document before. The images were demo except the dtb.
Because the board was made by ourselves according to the official design, and we could boot it from emmc or sd normally. What I changed at dts was " pcie0 disabled ".
But when it used NFS, there would be this problem. Do you have any idea ?
Best Regards,
Ida
Hi Ida J,
We are able to NFS boot the iMX8MQEVK using the below link:
Boot I.MX6q SABRE over the Network using TFTP and NFS
You can use the binary image as suggested by Igor.
Regards,
Karan Gajjar
Hi Ida
for narrowing down issue (if this is caused by custom board)
recommended to try to reproduce issue on nxp reference board
with demo images.
Best regards
igor