[iMX8MQ] How to Change a Mipi CSI2 Driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[iMX8MQ] How to Change a Mipi CSI2 Driver

1,286 Views
jhpark_vine
Contributor III

in I.MX8MQuad ,   as a Mipi CSI2 driver , we use  fsl,mxc-mipi-csi2_yav  (   mxc-mipi-csi2_yav.c ) 

This Mipi-CSI2 driver is used for OV5640 camera. 

but, in I.MX8M mini , to connect Sony IMX219 Camera sensor ,  they used fsl,imx8mm-mipi-csi driver  ( drivers/media/platform/mxc/capture/mxc_mipi_csi.c ) 

How can  use  fsl,imx8mm-mipi-csi   as a I.MX8MQuad Mipi CSI2 driver? 

  

====   fsl,imx8mm-mipi-csi    in IMX8M mini ===== 

mipi_csi_1: mipi_csi@32e30000 {
compatible = "fsl,imx8mm-mipi-csi";
reg = <0x32e30000 0x1000>;
interrupts = <GIC_SPI 17 IRQ_TYPE_LEVEL_HIGH>;
clock-frequency = <333000000>;
clocks = <&clk IMX8MM_CLK_CSI1_CORE>,
<&clk IMX8MM_CLK_CSI1_PHY_REF>,
<&clk IMX8MM_CLK_DISP_AXI_ROOT>,
<&clk IMX8MM_CLK_DISP_APB_ROOT>;
clock-names = "mipi_clk", "phy_clk", "disp_axi", "disp_apb";
bus-width = <4>;
power-domains = <&mipi_pd>;
status = "disabled";
};

 

 

=====  fsl,mxc-mipi-csi2_yav   in I.MX8MQ  =========

mipi_csi_1: mipi_csi1@30a70000 {
compatible = "fsl,mxc-mipi-csi2_yav";
reg = <0x30a70000 0x1000>;
interrupts = <GIC_SPI 44 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clk IMX8MQ_CLK_CSI1_CORE>,
<&clk IMX8MQ_CLK_CSI1_ESC>,
<&clk IMX8MQ_CLK_CSI1_PHY_REF>;
clock-names = "clk_core", "clk_esc", "clk_pxl";
assigned-clocks = <&clk IMX8MQ_CLK_CSI1_CORE>,
<&clk IMX8MQ_CLK_CSI1_PHY_REF>,
<&clk IMX8MQ_CLK_CSI1_ESC>;
#ifdef PIXEL_RAW // sony
assigned-clock-rates = <133000000>, <100000000>, <66000000>;
#else
assigned-clock-rates = <266000000>, <150000000>, <66000000>;
#endif
/*
assigned-clock-parents = <&clk IMX8MQ_SYS1_PLL_266M>,
<&clk IMX8MQ_SYS2_PLL_1000M>,
<&clk IMX8MQ_SYS1_PLL_800M>;
*/
power-domains = <&pgc_mipi_csi1>;
csis-phy-reset = <&src 0x4c 7>;
phy-gpr = <&iomuxc_gpr 0x88>;
status = "disabled";
};

 

0 Kudos
Reply
0 Replies